This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-3m [06 Nov 2018 12:02] – [Questions:] add LTSpice files Antoniu Miclaus | university:courses:electronics:electronics-lab-3m [23 Aug 2019 12:14] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: The MOS transistor connected as a diode ====== |
===== Objective: ===== | ===== Objective: ===== | ||
Line 26: | Line 26: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude and 0 offset. The differential scope channel 2 (2+, 2-) measures the current in the resistor (and in the transistor). The Single ended input of scope channel 1 (1+) is connected to measure the voltage across the transistor. The current flowing through the transistor is the voltage difference 2+ and 2- divided by the resistor value (100Ω). | + | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude |
{{: | {{: | ||
Line 56: | Line 56: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude and 0 offset. The differential scope channel 2 (2+, 2-) measures the current in the resistor (and in the transistor). The Single ended input of scope channel 1 (1-) is connected to measure the voltage across the transistor. The current flowing through the transistor is the voltage difference 2+ and 2- divided by the resistor value (100Ω). | + | The waveform generator should be configured for a 100 Hz triangle wave with 10 volt amplitude |
{{: | {{: | ||
Line 78: | Line 78: | ||
How do the V< | How do the V< | ||
+ | <WRAP round download> | ||
**Resources: | **Resources: | ||
+ | * Fritzing files: [[ https:// | ||
* LTSpice files: [[ https:// | * LTSpice files: [[ https:// | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||