This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-32 [25 Jan 2019 13:44] – add ltspice files Antoniu Miclaus | university:courses:electronics:electronics-lab-32 [05 Mar 2019 12:34] – [Other uses for this circuit:] Antoniu Miclaus | ||
---|---|---|---|
Line 92: | Line 92: | ||
There are other potential uses for a circuit that essentially allows current flow in only one direction with very low voltage drop across the switch. In battery chargers, where the input power source might be intermittent such as a solar panel or wind turbine generator, it is necessary to prevent the battery from discharging when the input power source is not generating a high enough voltage to charge the battery. Generally a simple Schottky diode is used for this purpose but as was pointed out in the background section this can lead to losses in efficiency. If an op amp with sufficiently low operating supply current is employed this can often be lower than the reverse leakage current in a large Schottky diode. | There are other potential uses for a circuit that essentially allows current flow in only one direction with very low voltage drop across the switch. In battery chargers, where the input power source might be intermittent such as a solar panel or wind turbine generator, it is necessary to prevent the battery from discharging when the input power source is not generating a high enough voltage to charge the battery. Generally a simple Schottky diode is used for this purpose but as was pointed out in the background section this can lead to losses in efficiency. If an op amp with sufficiently low operating supply current is employed this can often be lower than the reverse leakage current in a large Schottky diode. | ||
+ | <WRAP round download> | ||
**Resources: | **Resources: | ||
* Fritzing files: [[ https:// | * Fritzing files: [[ https:// | ||
* LTspice files: [[ https:// | * LTspice files: [[ https:// | ||
+ | </ | ||
**For Further Reading:** | **For Further Reading:** |