This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-30 [05 Mar 2019 12:37] – [Alternate component choices:] Antoniu Miclaus | university:courses:electronics:electronics-lab-30 [23 Aug 2019 14:04] – Antoniu Miclaus | ||
---|---|---|---|
Line 107: | Line 107: | ||
needed. | needed. | ||
- | Now configure both AWG channels as square waves with 5 V amplitudes and 2.5 V offsets ( 0 to 5 V | + | Now configure both AWG channels as square waves with 5 V amplitudes |
swings). Set AWG1 to a frequency of 1 KHz and AWG2 to a frequency of 2 KHz or twice AWG1. Be sure to set | swings). Set AWG1 to a frequency of 1 KHz and AWG2 to a frequency of 2 KHz or twice AWG1. Be sure to set | ||
the AWGs to run synchronously. | the AWGs to run synchronously. | ||
Line 158: | Line 158: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | Configure both AWG channels as square waves with 5 V amplitudes and 2.5 V offsets ( 0 to 5 V swings). | + | Configure both AWG channels as square waves with 5 V amplitudes |
Set both AWG1 and AWG2 to a frequency of 1 KHz. Also be sure to start with the phase of both AWG1 and | Set both AWG1 and AWG2 to a frequency of 1 KHz. Also be sure to start with the phase of both AWG1 and | ||
AWG2 set to 0°. Be sure to set the AWGs to run synchronously. | AWG2 set to 0°. Be sure to set the AWGs to run synchronously. |