This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-29 [05 Mar 2019 12:37] – [Alternate component choices:] Antoniu Miclaus | university:courses:electronics:electronics-lab-29 [23 Aug 2019 14:04] – Antoniu Miclaus | ||
---|---|---|---|
Line 62: | Line 62: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | Now configure both AWG channels as square waves with 5 V amplitudes. Set AWG1 to a frequency of 1 KHz and AWG2 to a frequency of 2 KHz or twice AWG1. Set the phase of AWG2 to 0 degrees. Be sure to set the AWGs to run synchronously. | + | Now configure both AWG channels as square waves with 5 V amplitudes |
Observe the Q output on the scope screen with respect to the signals seen at the CLK and D inputs. Capture the various waveforms and save a screen shot for inclusion in your lab report. | Observe the Q output on the scope screen with respect to the signals seen at the CLK and D inputs. Capture the various waveforms and save a screen shot for inclusion in your lab report. |