This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-28 [17 Jan 2021 19:47] – [For Further reading:] Doug Mercer | university:courses:electronics:electronics-lab-28 [13 Nov 2021 16:55] – [Hardware Setup:] Doug Mercer | ||
---|---|---|---|
Line 39: | Line 39: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 5V amplitude peak-to-peak and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. | + | Configure the waveform generator for a 100 Hz triangle wave with 5V amplitude peak-to-peak and 2.5V offset. Both scope channels should be set to 1V/Div. Configure the scope in XY mode with channel 1 on the horizontal axis and channel 2 on the vertical axis. |
{{ : | {{ : | ||