This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-27 [27 Oct 2017 08:44] – Trecia Agoylo | university:courses:electronics:electronics-lab-27 [25 Jan 2019 10:46] – [For Further Reading:] add Frizting files Antoniu Miclaus | ||
---|---|---|---|
Line 53: | Line 53: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used. The breadboard connections are shown in figure below. | Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used. The breadboard connections are shown in figure below. | ||
- | {{ : | + | {{ : |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 70: | Line 70: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used. The breadboard connections are shown in figure below. | Connect your circuit to the ADALM2000 I/O connector as indicated by the green boxes. It is best to ground the unused negative scope inputs when not being used. The breadboard connections are shown in figure below. | ||
- | {{ : | + | {{ : |
- | <WRAP centeralign> | + | <WRAP centeralign> |
==== Procedure: ==== | ==== Procedure: ==== | ||
Configure waveform generators, W1, with 100 Hz triangle wave with 0 V offset and 6 V amplitude values and W2, 100 Hz triangle wave with 0 V offset and 6 V amplitude values and 90° phase. Use the oscilloscope to observe the output of the circuit, CH2. | Configure waveform generators, W1, with 100 Hz triangle wave with 0 V offset and 6 V amplitude values and W2, 100 Hz triangle wave with 0 V offset and 6 V amplitude values and 90° phase. Use the oscilloscope to observe the output of the circuit, CH2. | ||
Line 141: | Line 141: | ||
The output circuitry of a typical TTL logic gate is commonly referred to a totem-pole output because the two output transistors are stacked one above the other like carvings on a totem pole. Is a gate circuit with a totem-pole output stage able to source load current, sink load current, or do both? | The output circuitry of a typical TTL logic gate is commonly referred to a totem-pole output because the two output transistors are stacked one above the other like carvings on a totem pole. Is a gate circuit with a totem-pole output stage able to source load current, sink load current, or do both? | ||
+ | |||
+ | *Resources: | ||
+ | * Fritzing files: [[ https:// | ||
=====For Further Reading: | =====For Further Reading: |