Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
university:courses:electronics:electronics-lab-24m [23 Mar 2017 16:48] – [Directions:] Doug Mercer | university:courses:electronics:electronics-lab-24m [24 Apr 2017 08:52] – rename Antoniu Miclaus |
---|
===== Directions: ===== | ===== Directions: ===== |
| |
Construct the circuit as shown in figure 1 on your solder-less breadboard. The green boxes indicate connections to the ADALM2000. Note: there is no input from the Discovery board just the power supply. The first inverting amplifier stage consists of M<sub>1</sub> with R<sub>1</sub> and the Red LED serving as the output load. The second inverting amplifier stage consists of M<sub>2</sub> with R<sub>2</sub> and the Green LED serving as the load. C<sub>1</sub> couples the output of the first stage at the drain of M<sub>1</sub> to the input of the second stage at the gate of M<sub>2</sub>. Similarly, C<sub>2</sub> couples the output of the second stage at the drain of M<sub>2</sub> back to the input of the first stage at the gate of M<sub>1</sub>. | Construct the circuit as shown in figure 1 on your solder-less breadboard. The green boxes indicate connections to the ADALM2000. Note: there is no input from the ADALM2000 board just the power supply. The first inverting amplifier stage consists of M<sub>1</sub> with R<sub>1</sub> and the Red LED serving as the output load. The second inverting amplifier stage consists of M<sub>2</sub> with R<sub>2</sub> and the Green LED serving as the load. C<sub>1</sub> couples the output of the first stage at the drain of M<sub>1</sub> to the input of the second stage at the gate of M<sub>2</sub>. Similarly, C<sub>2</sub> couples the output of the second stage at the drain of M<sub>2</sub> back to the input of the first stage at the gate of M<sub>1</sub>. |
| |
{{ :university:courses:electronics:a24m_f1.png?500 |}} | {{ :university:courses:electronics:a24m_f1.png?500 |}} |