This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-24m [14 Dec 2012 21:15] – [For further reading:] Doug Mercer | university:courses:electronics:electronics-lab-24m [23 Mar 2017 16:46] – [Directions:] Doug Mercer | ||
---|---|---|---|
Line 13: | Line 13: | ||
===== Materials: ===== | ===== Materials: ===== | ||
- | Analog Discovery Lab hardware\\ | + | ADALM2000 Active Learning Module\\ |
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
Jumper wires\\ | Jumper wires\\ | ||
- | 2 - 470Ω Resistors\\ | + | 2 - 470 Ω Resistors\\ |
- | 2 - 20KΩ Resistors\\ | + | 2 - 20 KΩ Resistors\\ |
- | 2 - 10KΩ Resistors\\ | + | 2 - 10 KΩ Resistors\\ |
2 - small signal NMOS transistors (ZVN2110A)\\ | 2 - small signal NMOS transistors (ZVN2110A)\\ | ||
1 - Red LED\\ | 1 - Red LED\\ | ||
1 - Green LED\\ | 1 - Green LED\\ | ||
- | 2 - 47uF Capacitors\\ | + | 2 - 47 uF Capacitors |
===== Directions: ===== | ===== Directions: ===== | ||
- | Construct the circuit as shown in figure 1 on your solder-less breadboard. The green boxes indicate connections to the Discovery hardware. Note: there is no input from the Discovery board just the power supply. The first inverting amplifier stage consists of M< | + | Construct the circuit as shown in figure 1 on your solder-less breadboard. The green boxes indicate connections to the ADALM2000. Note: there is no input from the Discovery board just the power supply. The first inverting amplifier stage consists of M< |
{{ : | {{ : | ||
Line 53: | Line 53: | ||
===== Materials: ===== | ===== Materials: ===== | ||
- | Analog Discovery Lab hardware\\ | + | ADALM2000 Active Learning Module\\ |
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
Jumper wires\\ | Jumper wires\\ | ||
- | 2 - 470Ω Resistors\\ | + | 2 - 470 Ω Resistors\\ |
- | 1 - 1KΩ Resistors\\ | + | 1 - 1 KΩ Resistors\\ |
- | 1 - 20KΩ Resistor\\ | + | 1 - 20 KΩ Resistor\\ |
- | 1 - 10KΩ Resistor\\ | + | 1 - 10 KΩ Resistor\\ |
- | 1 - 47KΩ Resistor\\ | + | 1 - 47 KΩ Resistor\\ |
1 - small signal diode (1N914)\\ | 1 - small signal diode (1N914)\\ | ||
2 - small signal NMOS transistors (ZVN2110A)\\ | 2 - small signal NMOS transistors (ZVN2110A)\\ | ||
1 - Red LED\\ | 1 - Red LED\\ | ||
1 - Green LED\\ | 1 - Green LED\\ | ||
- | 1 - 47uF Capacitor\\ | + | 1 - 47 uF Capacitor |
===== Directions: ===== | ===== Directions: ===== | ||
- | Construct the circuit as shown in figure 2 on your solder-less breadboard. The green boxes indicate connections to the Discovery hardware. Starting with the circuit from experiment 1, remove one of the 20K? resistors (old R< | + | Construct the circuit as shown in figure 2 on your solder-less breadboard. The green boxes indicate connections to the ADALM2000. Starting with the circuit from experiment 1, remove one of the 20K? resistors (old R< |
{{ : | {{ : |