This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:electronics-lab-20 [27 Oct 2017 10:19] – added breadboard circuits and scopy shots Dann Kristofer Bautista | university:courses:electronics:electronics-lab-20 [02 Feb 2023 21:16] (current) – [Activity: CMOS Amplifier stages] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Activity | + | ====== Activity: CMOS Amplifier stages |
===== Objective: ===== | ===== Objective: ===== | ||
Line 5: | Line 5: | ||
The goal is to explore a high gain inverting amplifier constructed from complementary MOS devices. | The goal is to explore a high gain inverting amplifier constructed from complementary MOS devices. | ||
- | ====== | + | ====== High gain inverting amplifier====== |
===== Materials: ===== | ===== Materials: ===== | ||
Line 43: | Line 43: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz triangle wave with 4V amplitude and 2.5V offset. Both scope channels should be set to 1V/Div. If you are using the CD4069A on the plus and minus power supplies you will need to use a larger 8V amplitude and 0V offset. | + | Configure the waveform generator for a 1 KHz triangle wave with 4V amplitude |
- | {{ : | + | {{ : |
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 55: | Line 55: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | ====== | + | ====== Adding negative feedback ====== |
- | On your solder-less breadboard construct the amplifier circuit shown in figure | + | On your solder-less breadboard construct the amplifier circuit shown in figure |
{{ : | {{ : | ||
Line 65: | Line 65: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz sine wave with 2V amplitude and 0V offset. Both scope channels should be set to 1V/Div. | + | Configure the waveform generator for a 1 KHz sine wave with 2V amplitude |
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== Procedure: ===== | ===== Procedure: ===== | ||
- | Apply a sinusoidal signal of 2V amplitude with zero offset voltage to the input and measure the gain of the entire system from 10 to 100 KHz. Use the Network (Bode) analyzer to plot gain and phase vs. frequency for the entire system. | + | Apply a sinusoidal signal of 2V amplitude |
+ | Figure 8 Plot for single stage amplifier using CD4007 </ | ||
===== Questions: ===== | ===== Questions: ===== | ||
Line 78: | Line 80: | ||
What is the gain from the input source, W1, to the output seen at the inverter output? Which components set this gain and why? | What is the gain from the input source, W1, to the output seen at the inverter output? Which components set this gain and why? | ||
- | ====== | + | ====== |
- | On your solder-less breadboard construct the amplifier circuit shown in figure | + | On your solder-less breadboard construct the amplifier circuit shown in figure |
{{ : | {{ : | ||
Line 88: | Line 90: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | Configure the waveform generator for a 1 KHz sine wave with 2V amplitude and 0V offset. Both scope channels should be set to 1V/Div. | + | Configure the waveform generator for a 1 KHz sine wave with 2V amplitude |
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
===== Procedure: ===== | ===== Procedure: ===== | ||
- | Apply a sinusoidal signal of 2V amplitude with zero offset voltage to the input and measure the gain of the entire system from 10 to 100 KHz. Use the Network (Bode) analyzer to plot gain and phase vs. frequency for the entire system. | + | Apply a sinusoidal signal of 2V amplitude |
+ | <WRAP centeralign> | ||
===== Questions: ===== | ===== Questions: ===== | ||
- | ====== | + | ====== |
- | In this part of the lab activity, the CD4069A(UB) un-buffered hex CMOS inverter and a CD4066 Quad analog switch are used as elements of a chopper amplifier. Reconnect the breadboard as indicated in figure | + | In this part of the lab activity, the CD4069A(UB) un-buffered hex CMOS inverter and a CD4066 Quad analog switch are used as elements of a chopper amplifier. Reconnect the breadboard as indicated in figure |
In operation, the input signal is modulated by the input switches, amplified by the ac amplifier, and then demodulated by the output switches. The 20 kΩ, 560 pF low pass filter minimizes the high frequency ripple in the output. | In operation, the input signal is modulated by the input switches, amplified by the ac amplifier, and then demodulated by the output switches. The 20 kΩ, 560 pF low pass filter minimizes the high frequency ripple in the output. | ||
Line 106: | Line 109: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
==== AC Amplifier Response to Pulse Modulated Signals ==== | ==== AC Amplifier Response to Pulse Modulated Signals ==== | ||
Line 114: | Line 117: | ||
==== Chopper Amplifier DC Transfer Characteristic ==== | ==== Chopper Amplifier DC Transfer Characteristic ==== | ||
- | Measure the transfer characteristic (DC gain) of the chopper amplifier by applying DC voltages between about -2 V and +2 V to the input and measuring the output. This can be done manually using waveform generator W1 with a DC wave shape and setting the offset. Be sure to take sufficient data to determine the linear and nonlinear ranges of the transfer characteristic. To reduce data taking time, try using the waveform generator to provide a very low frequency (100 Hz) triangle signal with 0V offset. For example, a 4V amplitude setting will give outputs between +2V and -2V, respectively. | + | Measure the transfer characteristic (DC gain) of the chopper amplifier by applying DC voltages between about -2 V and +2 V to the input and measuring the output. This can be done manually using waveform generator W1 with a DC wave shape and setting the offset. Be sure to take sufficient data to determine the linear and nonlinear ranges of the transfer characteristic. To reduce data taking time, try using the waveform generator to provide a very low frequency (100 Hz) triangle signal with 0V offset. For example, a 4V amplitude |
==== Chopper Amplifier Frequency Response ==== | ==== Chopper Amplifier Frequency Response ==== | ||
- | Apply a sinusoidal signal of 400mV amplitude with zero offset voltage to the input and measure the gain of the entire system from 10 to 100 KHz. Use the Network (Bode) analyzer to plot gain and phase vs. frequency for the entire system, paying special attention to the 50KHz to 100KHz range and the region near the frequency of the chopping clock. | + | Apply a sinusoidal signal of 400mV amplitude |
==== Chopper Amplifier Results ==== | ==== Chopper Amplifier Results ==== | ||
Line 130: | Line 133: | ||
==== For Further Study: ==== | ==== For Further Study: ==== | ||
- | ADI Mini Tutorial on [[http:// | + | ADI Mini Tutorial on [[adi>static/ |
===== Circuit Additions: ===== | ===== Circuit Additions: ===== | ||
Line 161: | Line 164: | ||
These three inverters can be used to construct the three stage amplifier in section 20.3 for example. | These three inverters can be used to construct the three stage amplifier in section 20.3 for example. | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||