This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-1st [05 Mar 2019 10:53] – [Additional Background on settling time measurements:] Antoniu Miclaus | university:courses:electronics:electronics-lab-1st [15 Sep 2019 19:25] – [For further reading:] Doug Mercer | ||
---|---|---|---|
Line 29: | Line 29: | ||
1 OP27 op-amp\\ | 1 OP27 op-amp\\ | ||
1 OP37 op-amp\\ | 1 OP37 op-amp\\ | ||
- | 1 OP97 ( slow settling amplifier | + | 1 OP97 ( slow settling amplifier )\\ |
2 0.1uF Capacitors (used to de-couple the Vp and Vn power supplies)\\ | 2 0.1uF Capacitors (used to de-couple the Vp and Vn power supplies)\\ | ||
Line 48: | Line 48: | ||
==== Hardware Setup: ==== | ==== Hardware Setup: ==== | ||
- | Waveform generator 1 should be configured for a 60 KHz square wave 1V amplitude and 0 volt offset. Scope channel 1 is used to monitor the input square wave and should be set to 500 mV/div and used as the trigger source. Scope channel 2 is used to alternately measure the op amp output, V< | + | Waveform generator 1 should be configured for a 60 KHz square wave 1V amplitude |
<WRAP centeralign> | <WRAP centeralign> | ||
Line 59: | Line 59: | ||
Next replace the OP27 amplifier with a OP37 amplifier from the Parts Kit. Again export the Error waveform showing the settling to both rising and falling input steps for inclusion in your Lab report. Overlay the OP37 settling waveform with the saved reference waveform of the OP27. Compare the settling time and general characteristics of each. You should also again store the Error waveform, scope channel 2, for the OP37 as a reference waveform (R2) for future comparison. | Next replace the OP27 amplifier with a OP37 amplifier from the Parts Kit. Again export the Error waveform showing the settling to both rising and falling input steps for inclusion in your Lab report. Overlay the OP37 settling waveform with the saved reference waveform of the OP27. Compare the settling time and general characteristics of each. You should also again store the Error waveform, scope channel 2, for the OP37 as a reference waveform (R2) for future comparison. | ||
- | Finally replace the OP37 with the much slower settling OP97 amplifier | + | Finally replace the OP37 with the much slower settling OP97 amplifier. Again export the Error waveform showing the settling to both rising and falling input steps for inclusion in your Lab report. Overlay the OP97 settling waveform with the saved reference waveforms of the OP27 and OP37. Compare the settling time and general characteristics of each. |
{{ : | {{ : | ||
Line 97: | Line 97: | ||
http:// | http:// | ||
http:// | http:// | ||
- | http:// | + | [[wp>Settling_time|Settling time]] |
Return to Lab Activities [[university: | Return to Lab Activities [[university: | ||