This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-14 [12 Jul 2019 13:59] – [Activity 14: R-2R Resistor Ladder Digital to Analog Converter] Pop Andreea | university:courses:electronics:electronics-lab-14 [24 Sep 2019 10:22] – [Questions:] Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity: | + | ======Activity: |
- | + | =====R-2R Resistor Ladder Digital to Analog Converter===== | |
- | =====Objective: | + | ====Objective: |
The objective of this exercise is to explore the concepts of digital to analog conversion making use of the CMOS inverter as reference switches for a resistor ladder divider (used in DAC). | The objective of this exercise is to explore the concepts of digital to analog conversion making use of the CMOS inverter as reference switches for a resistor ladder divider (used in DAC). | ||
- | =====Background: | + | ====Background: |
We will exploit the simple CMOS inverter logic gate as a pair of switches. The digital I/O signals of the ADALM2000 module can be configured as standard CMOS dividers with a +3.3 Volt supply (push-pull mode). In the simplest form, a CMOS output consists of one PMOS device, M< | We will exploit the simple CMOS inverter logic gate as a pair of switches. The digital I/O signals of the ADALM2000 module can be configured as standard CMOS dividers with a +3.3 Volt supply (push-pull mode). In the simplest form, a CMOS output consists of one PMOS device, M< | ||
Line 15: | Line 15: | ||
When used in what is referred to as " | When used in what is referred to as " | ||
- | =====Materials: | + | ====Materials: |
ADALM2000 Active Learning Module\\ | ADALM2000 Active Learning Module\\ | ||
Solder-less breadboard\\ | Solder-less breadboard\\ | ||
Line 23: | Line 23: | ||
1 - OP27 amplifier | 1 - OP27 amplifier | ||
- | =====Directions: | + | ====Directions: |
Build the 8 bit resister ladder circuit shown in figure 2, preferably on your solder-less breadboard. The number of resistors normally supplied in the Analog Parts Kit is not sufficient to build the full 8 bit ladder. It is best to use 1% resistors for this project if you have access to them. | Build the 8 bit resister ladder circuit shown in figure 2, preferably on your solder-less breadboard. The number of resistors normally supplied in the Analog Parts Kit is not sufficient to build the full 8 bit ladder. It is best to use 1% resistors for this project if you have access to them. | ||
Line 33: | Line 33: | ||
Connect the 8 digital outputs designated by the blue boxes, and the scope channel and AWG output designated by the green boxes to the resistor ladder circuit as shown. Remember to connect power to the op amp supply pins. | Connect the 8 digital outputs designated by the blue boxes, and the scope channel and AWG output designated by the green boxes to the resistor ladder circuit as shown. Remember to connect power to the op amp supply pins. | ||
- | =====Hardware Setup:===== | + | ====Hardware Setup:==== |
{{ : | {{ : | ||
Line 39: | Line 39: | ||
<WRAP centeralign > Figure 3 R-2R Resistor Ladder Circuit Breadboard Connections </ | <WRAP centeralign > Figure 3 R-2R Resistor Ladder Circuit Breadboard Connections </ | ||
- | =====Proceduce:===== | + | ====Procedure:==== |
With both R< | With both R< | ||
Line 57: | Line 57: | ||
Here are some pre-made waveform files you can try: Sine, Triangle, Gaussian pulse etc. [[ https:// | Here are some pre-made waveform files you can try: Sine, Triangle, Gaussian pulse etc. [[ https:// | ||
+ | =====AD5626 12-bit nanoDAC===== | ||
+ | |||
+ | =====Background===== | ||
+ | AD5626 is a vltage output digital-to-analog converter that can operate from a single 5V supply. | ||
+ | the DAC, input shift register and latches, reference, and a rail to-rail output amplifier which can swing to either rail and is set to a | ||
+ | range of 0 V to 4.095 V for a one-millivolt-per-bit resolution. | ||
+ | This part features a serial interface that is high speed, threewire, DSP compatible with data in (SDIN), clock (SCLK), and | ||
+ | load strobe (LDAC). There is also a chip-select pin for connecting multiple DACs. | ||
+ | The CLR input sets the output to zero scale at power on or upon user demand. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 6. functional block diagram of AD5626 </ | ||
+ | |||
+ | The AD5626 has a separate serial input register from the 1-bit DAC register and it allows preloading of a new data value into the serial register without disturbing the present DAC output voltage. | ||
+ | the loaded value can be transferred to the DAC register by strobing the LDAC pin. | ||
+ | ===== Unipolar output operation===== | ||
+ | This mode of operation is the basic mode for AD5626. You can verify the god functionality AD5626 according to the unipolar code table of the digital to analog convertor. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 7. Unipolar code table of AD5626</ | ||
+ | ====Materials==== | ||
+ | ADALM2000 Active Learning Module\\ | ||
+ | Solder-less breadboard\\ | ||
+ | Jumper wires\\ | ||
+ | 1 - AD5626 12-bit nanoDAC\\ | ||
+ | 1 - 2.2 KΩ resistor\\ | ||
+ | 1 - 0.001 uF capacitor\\ | ||
+ | 1 - 0.1 uF capacitor\\ | ||
+ | 1 - 10 uF capcitor\\ | ||
+ | |||
+ | ====Hardware setup==== | ||
+ | Connect the pins of AD5626 as shown in figure 8. | ||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 8. Connections for Unipolar operation AD5626</ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 9. AD5626 breadboard connections</ | ||
+ | |||
+ | |||
+ | ====Procedure==== | ||
+ | Open Scopy and enable the positive power supply to 5V. in Pattern generator you should configure the DAC input signals according to the timing diagram of AD5626 presented in datasheet. | ||
+ | Start by configuring SPI signals. Create a group channel with DIO0, DIO1 and DIO2. If the connections were done as in figure 8 then DIO0 is the clock signal, DIO2 the data signal and DIO0 the /CS signal. | ||
+ | It is specified in datasheet that the clock width for both high and low states should be at least 30 ns. From this you can compute the clock period and therefore maximum frequency. | ||
+ | Set the clock frequency to 1Mhz. Set CLK Polarity and CLK Phase to 1. | ||
+ | |||
+ | As the AD5626 is a 12-bit DAC, the data sent through SPI should be aleast 12 bits long. Set the number of Bytes per frame to 2 and it will send 16 bits when the conversion is initiated. | ||
+ | In the Data text box you can enter the value to be sent to the ADC. | ||
+ | The signals of the SPI group channel should resemble the timing diagram of the AD5626 digital to analog converter. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 10. AD5626 SPI timing diagram</ | ||
+ | |||
+ | Now you should configure /LDAC and /CLR signals. | ||
+ | From the datasheet we know that the shift register contents are updated on the rising edge of /LDAC if /CLR is high. | ||
+ | Set the pattern of DIO4 (/CLR) as " | ||
+ | /LDAC signal(DIO3) should have a rising edge before /CS falling egde and should be high as long as bits are transmitted serially. | ||
+ | In order to fulfill tre previoulsy stated conditions, DIO3 signal can be set at 13kHz frequency and 160 degrees phase. | ||
+ | In figure 10 are presented all the input signals needed for AD5626 digital to analog conversion. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign > Figure 11. Pattern generator signals setup</ | ||
+ | |||
+ | The last step is to open oscilloscope and connect channel 1 to the output of AD5626. Enable channel 1 measurements and enter a value in the " | ||
+ | In figure 12 you can see the output voltage if the data sent through SPI is 7FF. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 12. AD5626 output voltage for 7FF input.</ | ||
+ | |||
+ | ===== Bipolar output operation===== | ||
+ | Although the AD5626 has been designed for single-supply operation, bipolar operation is achievable using the circuit | ||
+ | illustrated in Figure 13. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 13. Bipolar output operation without trim</ | ||
+ | |||
+ | This circuit can be used for applications that do not require high accuracy. | ||
+ | voltage is coded in offset binary and is given by: | ||
+ | \\ | ||
+ | < | ||
+ | |||
+ | \\ | ||
+ | For the ±5V output range and the circuit values shown in the table in figure 13 the transfer equation becomes: | ||
+ | \\ | ||
+ | < | ||
+ | \\ | ||
+ | |||
+ | ====Materials==== | ||
+ | ADALM2000 Active Learning Module\\ | ||
+ | Solder-less breadboard\\ | ||
+ | Jumper wires\\ | ||
+ | 1 - AD5626 12-bit nanoDAC\\ | ||
+ | 1 - 0.1 uF capacitor\\ | ||
+ | 1 - 1 KΩ resistor\\ | ||
+ | 1 - 20 KΩ resistor\\ | ||
+ | 2 - 10 KΩ resistors\\ | ||
+ | 1 - 47 KΩ resistor\\ | ||
+ | 1 - 470 KΩ resistor\\ | ||
+ | ====Hardware setup==== | ||
+ | Build the circuit presented in figure 13 on your solderless breadboard. | ||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 14. AD5626 Bipolar output operation breadboard connections</ | ||
+ | |||
+ | ====Procedure==== | ||
+ | You can configure the DAC for unipolar output operation as described above. For the voltage reference use the channel 1 of the Signal generator | ||
+ | On the second channel of the oscilloscope visualize the voltage at the output of the opamp. | ||
+ | You can visualize both the voltages for unipolar operation and bipolar operation at the same time on the oscilloscope. | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 15. Unipolar and Bipolar output voltage for 000 input</ | ||
+ | |||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 16. Unipolar and Bipolar output voltage for 800 input</ | ||
+ | {{ : | ||
+ | <WRAP centeralign > Figure 17. Unipolar and Bipolar output voltage for FFF input</ | ||
=====Questions: | =====Questions: | ||
Line 74: | Line 189: | ||
<WRAP round download> | <WRAP round download> | ||
**Resources: | **Resources: | ||
- | * Fritzing files: [[ https:// | + | * Fritzing files: [[ https:// |
- | * LTspice files: [[ https:// | + | * LTspice files: [[ https:// |
</ | </ | ||