This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:electronics-lab-11 [23 Mar 2017 16:17] – [Materials:] Doug Mercer | university:courses:electronics:electronics-lab-11 [24 Jul 2017 15:27] – change amplitude value to peak-peak Antoniu Miclaus | ||
---|---|---|---|
Line 22: | Line 22: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz Sine wave with 2 volt amplitude and 0 offset. The Single ended input of scope channel 2 (2+) is used to measure the voltage at the emitter. The Scope configured with channel 1+ connected to display the AWG generator output. When measuring the input to output error, channel 2 of the scope should be connected to display 2+ and 2- differential. | + | The waveform generator should be configured for a 1 KHz Sine wave with 4 volt amplitude and 0 offset. The Single ended input of scope channel 2 (2+) is used to measure the voltage at the emitter. The Scope configured with channel 1+ connected to display the AWG generator output. When measuring the input to output error, channel 2 of the scope should be connected to display 2+ and 2- differential. |
{{ : | {{ : | ||
Line 71: | Line 71: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz Sine wave with 1 volt amplitude with the offset set equal to minus the V< | + | The waveform generator should be configured for a 1 KHz Sine wave with 2 volt amplitude with the offset set equal to minus the V< |
===== Procedure: ===== | ===== Procedure: ===== | ||
Line 98: | Line 98: | ||
===== Hardware Setup: ===== | ===== Hardware Setup: ===== | ||
- | The waveform generator should be configured for a 1 KHz Sine wave with 1 volt amplitude with the offset set equal to 0. Scope input channel 2 is set to 500mV / Div. | + | The waveform generator should be configured for a 1 KHz Sine wave with 2 volt amplitude with the offset set equal to 0. Scope input channel 2 is set to 500mV / Div. |
===== Procedure: ===== | ===== Procedure: ===== |