Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:electronics:electronics-lab-10 [12 Nov 2018 12:36] – Antoniu Miclaus | university:courses:electronics:electronics-lab-10 [23 Aug 2019 13:05] – Antoniu Miclaus |
---|
====== Activity 10. Shunt regulator ====== | ====== Activity: Shunt regulator ====== |
| |
===== Objective: ===== | ===== Objective: ===== |
<WRAP centeralign> Figure 2 Band-gap shunt regulator Breadboard Circuit </WRAP> | <WRAP centeralign> Figure 2 Band-gap shunt regulator Breadboard Circuit </WRAP> |
| |
Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the regulated output voltage at the collector of Q<sub>3</sub>. | Waveform generator W1 should be configured for a 1 KHz triangle wave with 4 volt amplitude peak-to-peak and 2V offset. The Single ended input of scope channel 2 (2+) is used to measure the regulated output voltage at the collector of Q<sub>3</sub>. |
| |
===== Procedure: ===== | ===== Procedure: ===== |
All the emitters can be tired to ground ( pins 3,7,10,13 ). Devices Q<sub>1</sub>, Q<sub>2</sub> and Q<sub>3</sub> can be connected in parallel and serve as Q<sub>2</sub> in figure 1. Q<sub>4</sub> and Q<sub>5</sub> can be used for Q<sub>1</sub> and Q<sub>3</sub> in figure 2. The 3 to 1 emitter area ratio will result in an output voltage very nearly 1.2 volts if R<sub>1</sub> and R<sub>3</sub> are both equal to 2KΩ. | All the emitters can be tired to ground ( pins 3,7,10,13 ). Devices Q<sub>1</sub>, Q<sub>2</sub> and Q<sub>3</sub> can be connected in parallel and serve as Q<sub>2</sub> in figure 1. Q<sub>4</sub> and Q<sub>5</sub> can be used for Q<sub>1</sub> and Q<sub>3</sub> in figure 2. The 3 to 1 emitter area ratio will result in an output voltage very nearly 1.2 volts if R<sub>1</sub> and R<sub>3</sub> are both equal to 2KΩ. |
| |
| <WRAP round download> |
**Resources:** | **Resources:** |
| * Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/fritzing/shunt_volt_reg_bb | shunt_reg_bb]] |
* LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/shunt_reg_ltspice | shunt_reg_ltspice]] | * LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m2k/ltspice/shunt_reg_ltspice | shunt_reg_ltspice]] |
| </WRAP> |
| |
**Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** | **Return to Lab Activity [[university:courses:electronics:labs|Table of Contents]]** |
| |