This is an old revision of the document!
The objective of this lab activity is to examine polyphase filter circuits as a quadrature generation technique and to extend the differential tuned amplifier to create a polyphase amplifier or filter that can produce all four quadrature ( 90º increments ) phases of an input signal source.
The use of quadrature frequency conversion is common in modern wireless transceiver architectures, because both amplitude modulation and phase modulation are deployed in today's digital communication systems.
http://en.wikipedia.org/wiki/Quadrature_amplitude_modulation
Figure 1 shows a simplified first order polyphase circuit, as implemented in many quadrature demodulators such as the ADL5380. This simple polyphase circuit consists of complementary RC subcircuits. A low-pass transfer function from the input to one output shifts the phase by -45º at the corner frequency, and a high-pass transfer function to the other output shifts the phase by +45º at the corner frequency. The net phase difference between the two outputs will be 90º. If the R and C values of the two paths are matched, then both paths have the same corner frequency and, more importantly, the phase of one output tracks the other with a 90° phase shift for all frequencies. The relative amplitudes of the two output signals, ( LO I 0º and LO Q 90º ) will be only equal at the -3dB corner frequency of the two RC paths.
Figure 1. Simplified First Order Polyphase Filter
Generation of quadrature local oscillator (LO) signals is an important functional block in sideband rejection heterodyne receivers. Quadrature accuracy, that is the phase accuracy of the in phase and quadrature 90º phase-shifted signals, directly determines the image reject ratio (IRR), an important specification determining the sensitivity of a receiver.
ADALM2000 Active Learning Module
Solder-less breadboard, and jumper wire kit
2 - 1 nF capacitors ( marked 102 )
2 - 1 KΩ resistors
Build the polyphase filter circuit shown in figure 2 on your solder-less breadboard.
Figure 2 polyphase filter circuit
The green squares indicate where to connect the ADALM2000 module AWG, and scope channels.
Open the Network Analyzer software tool in Scopy. Configure the frequency sweep to start at 10 KHz and stop at 10 MHz. Set the amplitude to 1 V and the offset to zero. Check the box “Use Channel 1 as reference” under the scope channels drop down menu to measure the phase of one output path with respect to the other.
Calculate the expected RC corner frequency based on the R and C values you used. Run a single sweep of the frequency and be sure to save your data to a .csv file for later use in either MatLAB or Excel.
By adding second order L-C and C-L low and high pass filter sections as differential output loads in a NPN differential amplifier we can generate all four 90º phases ( i.e. 0º, 90º, 180º and 270º ) of an input sine wave signal. Such a tuned amplifier is shown in figure 3.
ADALM2000 Active Learning Module
Solder-less breadboard, and jumper wire kit
1 - SSM2212 NPN matched transistor pair ( Q1, Q2 )
2 - 2N3904 NPN transistors ( Q3, Q4 )
2 - 100 uH inductor (Various other value inductors)
2 - 1 nF capacitors ( marked 102 )
2 - 0.1 uF capacitors ( marked 104 )
2 - 10 Ω resistors
2 - 150 Ω resistors
2 - 470 Ω resistors
3 - 1 KΩ resistors
1 - 10 KΩ resistor
Other resistor and capacitors as needed
Build the circuit shown in figure 3 on your solder-less breadboard. Use the SSM2212 matched transistor pair for Q1 and Q2. Transistors Q3 and Q4 can be 2N3904 devices. Set L1 = L2 = 100 uH and C1 = C2 = 1nF. R1 should be equal to R2 and use 470 Ω for their value. Likewise, R3 should be equal to R4 and use 150 Ω for their value.
Figure 3 Polyphase Amplifier
The green squares indicate where to connect the Discovery module AWG, scope channels and power supplies. Be sure to turn on the power supplies only after you double check your wiring.
Open the voltage supply control window to turn on and off the fixed +5 and -5 volt power supplies. Open the Network Analyzer software tool in Waveforms. Configure the frequency sweep to start at 10 KHz and stop at 10 MHz. Set the amplitude to 500 mV and the offset to zero.
Calculate the expected LC corner frequency based on the L and C values used.
Turn on the power supplies. Connect scope input channel 2 through an AC coupling capacitor ( C4 in figure 3 ) alternately to each of the four possible outputs at the ends of resistors R1, R2, R3 and R4. Run a single frequency sweep and store each sweep in a waveform snapshot to compare each output's relative gain and phase response. Be sure to export all the frequency sweep data to a .csv file for further analysis in either Excel or Matlab.
Using the scope and function generator software instruments ( in the time domain ) set the AWG frequency to the resonate frequency with the amplitude set to 500 mV. Trigger on scope channel 1. Observe the relative amplitudes and phases of the four outputs and store each waveform on channel 2 as a reference channel to compare the amplitude and phase of each output.
For Further Reading:
http://www.microwavejournal.com/ext/resources/pdf-downloads/IQTheory-of-Operation.pdf
Return to Lab Activity Table of Contents.