This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:electronics:comms-lab-polyphase-filter [27 Mar 2017 17:08] – [Hardware Setup:] Doug Mercer | university:courses:electronics:comms-lab-polyphase-filter [23 Aug 2019 15:13] – Antoniu Miclaus | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | |||
======Activity: | ======Activity: | ||
Line 35: | Line 36: | ||
The green squares indicate where to connect the ADALM2000 module AWG, and scope channels. | The green squares indicate where to connect the ADALM2000 module AWG, and scope channels. | ||
+ | {{ : | ||
- | Open the Network Analyzer software tool in Scopy. Configure the frequency sweep to start at 10 KHz and stop at 10 MHz. Set the amplitude to 1 V and the offset to zero. Check the box "Use Channel 1 as reference" | + | <WRAP centeralign> |
+ | |||
+ | Open the Network Analyzer software tool in Scopy. Configure the frequency sweep to start at 10 KHz and stop at 30 MHz. Set the amplitude to 2 V and the offset to zero. Check the box "Use Channel 1 as reference" | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
====Procedure: | ====Procedure: | ||
Line 47: | Line 54: | ||
=====Differential Polyphase Tuned Amplifier===== | =====Differential Polyphase Tuned Amplifier===== | ||
- | By adding second order L-C and C-L low and high pass filter sections as differential output loads in a NPN differential amplifier we can generate all four 90º phases ( i.e. 0º, 90º, 180º and 270º ) of an input sine wave signal. Such a tuned amplifier is shown in figure | + | By adding second order L-C and C-L low and high pass filter sections as differential output loads in a NPN differential amplifier we can generate all four 90º phases ( i.e. 0º, 90º, 180º and 270º ) of an input sine wave signal. Such a tuned amplifier is shown in figure |
====Materials: | ====Materials: | ||
Line 66: | Line 73: | ||
====Directions: | ====Directions: | ||
- | Build the circuit shown in figure | + | Build the circuit shown in figure |
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
====Hardware Setup:==== | ====Hardware Setup:==== | ||
The green squares indicate where to connect the ADALM2000 module AWG, scope channels and power supplies. Be sure to turn on the power supplies only after you double check your wiring. | The green squares indicate where to connect the ADALM2000 module AWG, scope channels and power supplies. Be sure to turn on the power supplies only after you double check your wiring. | ||
+ | {{ : | ||
- | Open the voltage supply control window to turn on and off the fixed +5 and -5 volt power supplies. Open the Network Analyzer software tool in Scopy. Configure the frequency sweep to start at 10 KHz and stop at 10 MHz. Set the amplitude to 500 mV and the offset to zero. | + | <WRAP centeralign> |
+ | |||
+ | Open the voltage supply control window to turn on and off the fixed +5 and -5 volt power supplies. Open the Network Analyzer software tool in Scopy. Configure the frequency sweep to start at 100 Hz and stop at 30 MHz. Set the amplitude to 1V and the offset to zero. | ||
====Procedure: | ====Procedure: | ||
Line 84: | Line 94: | ||
Turn on the power supplies. Connect scope input channel 2 through an AC coupling capacitor ( C< | Turn on the power supplies. Connect scope input channel 2 through an AC coupling capacitor ( C< | ||
- | Using the scope and function generator software instruments ( in the time domain ) set the AWG frequency to the resonate frequency with the amplitude set to 500 mV. Trigger on scope channel 1. Observe the relative amplitudes and phases of the four outputs and store each waveform on channel 2 as a reference channel to compare the amplitude and phase of each output. | + | Using the scope and function generator software instruments ( in the time domain ) set the AWG frequency to the resonate frequency with the amplitude set to 1V peak-to-peak. Trigger on scope channel 1. Observe the relative amplitudes and phases of the four outputs and store each waveform on channel 2 as a reference channel to compare the amplitude and phase of each output. |
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Resources: | ||
+ | * Fritzing files: [[ https:// | ||
+ | * LTspice files: [[ https:// | ||
+ | </ | ||
====Questions: | ====Questions: | ||
Line 94: | Line 121: | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||
+ | |||
+ | |||