This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:electronics:comms-lab-peltz-osc [27 Mar 2017 17:13] – [Directions:] Doug Mercer | university:courses:electronics:comms-lab-peltz-osc [05 Jan 2018 03:35] – Trecia Agoylo | ||
---|---|---|---|
Line 48: | Line 48: | ||
Set both scope inputs to 200 mV/div and the time base to 1 uSec/div. Set the trigger on the rising edge of channel 1. | Set both scope inputs to 200 mV/div and the time base to 1 uSec/div. Set the trigger on the rising edge of channel 1. | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Procedure: | =====Procedure: | ||
Turn on the -5V power supply. Observe the output waveform across the LC tank on scope channel 1. You can also observe the waveform seen at the emitters of Q< | Turn on the -5V power supply. Observe the output waveform across the LC tank on scope channel 1. You can also observe the waveform seen at the emitters of Q< | ||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
Notice that the output signal swings positive and negative around ground (0 V). Measure the frequency of the output waveform. Measure the peak to peak amplitude R< | Notice that the output signal swings positive and negative around ground (0 V). Measure the frequency of the output waveform. Measure the peak to peak amplitude R< | ||
Line 64: | Line 70: | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||
+ |