This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:electronics:comms-lab-colpitts-osc [27 Mar 2017 17:10] – [Materials:] Doug Mercer | university:courses:electronics:comms-lab-colpitts-osc [25 Jun 2020 22:07] (current) – external edit 127.0.0.1 | ||
---|---|---|---|
Line 49: | Line 49: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | The green squares indicate where to connect the Discovery module | + | <WRAP centeralign> |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The green squares indicate where to connect the ADALM2000module | ||
=====Procedure: | =====Procedure: | ||
Having finished construction the Colpitts oscillator check that the circuit is oscillating correctly by turning on both the + and - 5 V power supplies and connecting one of the oscilloscope channels to the output terminal. It may be found that the value of R< | Having finished construction the Colpitts oscillator check that the circuit is oscillating correctly by turning on both the + and - 5 V power supplies and connecting one of the oscilloscope channels to the output terminal. It may be found that the value of R< | ||
+ | |||
+ | A plot example using R< | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Questions: | =====Questions: | ||
Line 68: | Line 78: | ||
|50 uH| | | | |50 uH| | | | ||
|100 uH| | | | |100 uH| | | | ||
+ | |||
+ | <WRAP round download> | ||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[downgit> | ||
+ | * LTspice files: [[downgit> | ||
+ | </ | ||
**For Further Reading:** | **For Further Reading:** |