This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:comms-lab-clapp-osc [03 Sep 2014 20:43] – [Background:] Doug Mercer | university:courses:electronics:comms-lab-clapp-osc [26 Oct 2018 12:31] – [Questions:] add Fritzing files Antoniu Miclaus | ||
---|---|---|---|
Line 29: | Line 29: | ||
=====Materials: | =====Materials: | ||
- | + | ADALM2000 Active Learning Module\\ | |
- | Analog Discovery Lab hardware\\ | + | |
Solder-less breadboard, and jumper wire kit\\ | Solder-less breadboard, and jumper wire kit\\ | ||
1 - 2N3904 NPN transistor\\ | 1 - 2N3904 NPN transistor\\ | ||
Line 53: | Line 52: | ||
=====Hardware Setup:===== | =====Hardware Setup:===== | ||
- | The green squares indicate where to connect the Discovery | + | <WRAP centeralign> |
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | The green squares indicate where to connect the ADALM2000 | ||
=====Procedure: | =====Procedure: | ||
Having finished construction the Clapp oscillator check that the circuit is oscillating correctly by turning on both the + and - 5 V power supplies and connecting one of the oscilloscope channels to the output terminal. It may be found that the value of R< | Having finished construction the Clapp oscillator check that the circuit is oscillating correctly by turning on both the + and - 5 V power supplies and connecting one of the oscilloscope channels to the output terminal. It may be found that the value of R< | ||
+ | |||
+ | A plot example using R< | ||
+ | |||
+ | <WRAP centeralign> | ||
+ | |||
+ | <WRAP centeralign> | ||
=====Questions: | =====Questions: | ||
Line 72: | Line 81: | ||
|50 uH| | | | |50 uH| | | | ||
|100 uH| | | | |100 uH| | | | ||
+ | |||
+ | **Lab Resources: | ||
+ | * Fritzing files: [[ https:// | ||
**For Further Reading:** | **For Further Reading:** |