This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:electronics:buck_converter_basics [10 May 2019 20:15] – Add round download box [Circuit Construction and Testing] Mark Thoren | university:courses:electronics:buck_converter_basics [26 Mar 2020 00:38] – Add references to ADALM-BUCK board. Mark Thoren | ||
---|---|---|---|
Line 39: | Line 39: | ||
Solder-less breadboard and jumper wire kit or Perma Proto solder breadboard\\ | Solder-less breadboard and jumper wire kit or Perma Proto solder breadboard\\ | ||
ADALP2000 parts kit parts as required\\ | ADALP2000 parts kit parts as required\\ | ||
+ | Optional: [[university: | ||
12V power supply (preferred) or 5V USB power supply (workable)\\ | 12V power supply (preferred) or 5V USB power supply (workable)\\ | ||
Voltmeter (optional, can use M2K in Voltmeter mode.)\\ | Voltmeter (optional, can use M2K in Voltmeter mode.)\\ | ||
Line 145: | Line 146: | ||
==== Circuit Construction and Testing ==== | ==== Circuit Construction and Testing ==== | ||
Build the following breadboard circuit for the buck converter, following the schematic in Figure 16. (Q1, R2, R3 can be added later.) Note that the HPH1-1400L has six inductors that can be connected in any way (series, parallel, or a combination of the two). Be sure to observe proper polarity, connecting all inductors in series as shown. | Build the following breadboard circuit for the buck converter, following the schematic in Figure 16. (Q1, R2, R3 can be added later.) Note that the HPH1-1400L has six inductors that can be connected in any way (series, parallel, or a combination of the two). Be sure to observe proper polarity, connecting all inductors in series as shown. | ||
+ | <WRAP info> | ||
+ | The circuits in this lab are compatible with solderless breadboard construction. However they are relatively complicated and take time to construct and debug. The [[university: | ||
+ | </ | ||
{{ : | {{ : | ||
Line 230: | Line 234: | ||
===== Slide Deck ===== | ===== Slide Deck ===== | ||
A slide deck is provided as a companion to this exercise, and can be used to help in presenting this material in classroom, lab setting, or in hands-on workshops. | A slide deck is provided as a companion to this exercise, and can be used to help in presenting this material in classroom, lab setting, or in hands-on workshops. | ||
+ | <WRAP round download> | ||
{{ : | {{ : | ||
+ | </ | ||
**Return to Lab Activity [[university: | **Return to Lab Activity [[university: | ||