This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:alm1k:m2k-convert-labs [03 Nov 2018 17:32] – add link to input didver how-to page Doug Mercer | university:courses:alm1k:m2k-convert-labs [29 Jul 2019 02:03] – [Notes:] Doug Mercer | ||
---|---|---|---|
Line 11: | Line 11: | ||
For the ALM1000 module we use the following terminology when referring to the connections to the connector and configuring the hardware. The analog I/O channel pins are referred to as CA and CB. | For the ALM1000 module we use the following terminology when referring to the connections to the connector and configuring the hardware. The analog I/O channel pins are referred to as CA and CB. | ||
- | {{ : | + | {{ : |
- | <WRAP centeralign> | + | <WRAP centeralign> |
When configured to force voltage / measure current –V is added as in CA-V or when configured to force current / measure voltage –I is added as in CA-I. When a channel is configured in the high impedance mode to only measure voltage –H is added as CA-H. The fixed power and ground connections are referred as GND, +5 and +2.5. | When configured to force voltage / measure current –V is added as in CA-V or when configured to force current / measure voltage –I is added as in CA-I. When a channel is configured in the high impedance mode to only measure voltage –H is added as CA-H. The fixed power and ground connections are referred as GND, +5 and +2.5. |