This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
university:courses:alm1k:circuits1:alm-joule-thief [03 Jan 2021 22:12] – fix links Robin Getz | university:courses:alm1k:circuits1:alm-joule-thief [27 Jan 2021 22:36] – use wp> interwiki links Robin Getz | ||
---|---|---|---|
Line 142: | Line 142: | ||
To better investigate how the circuit operates we next need to break (open) the feedback loop and stop the circuit from oscillating. We can then inject a test signal at the base of the transistor as shown in figure 4. Add the modifications shown in figure 4 to your circuit. | To better investigate how the circuit operates we next need to break (open) the feedback loop and stop the circuit from oscillating. We can then inject a test signal at the base of the transistor as shown in figure 4. Add the modifications shown in figure 4 to your circuit. | ||
- | The voltage waveform on the secondary side of the transformer might go outside the 0 to +5 V range of the ALM1000 input. To observe the voltage waveform we can AC couple the signal and use a [[https:// | + | The voltage waveform on the secondary side of the transformer might go outside the 0 to +5 V range of the ALM1000 input. To observe the voltage waveform we can AC couple the signal and use a [[/ |
{{ : | {{ : | ||
Line 388: | Line 388: | ||
**For Further Reading:** | **For Further Reading:** | ||
- | [[http:// | + | [[wp>Boost_converter|Boost Converter]]\\ |
- | [[https:// | + | [[wp>Joule_thief|Joule Thief]]\\ |
- | [[https:// | + | [[wp>Sziklai_pair|Compound Transistor]] |
**Return to ALM Lab Activity [[university: | **Return to ALM Lab Activity [[university: | ||