This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:alm1k:circuits1:alm-cir-6 [06 Oct 2018 16:24] – [Activity 6: Transient Response of an RL Circuit] Doug Mercer | university:courses:alm1k:circuits1:alm-cir-6 [03 Nov 2021 20:14] (current) – [Activity: Transient Response of an RL Circuit] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity: | + | ======Activity: |
=====Objective: | =====Objective: | ||
Line 82: | Line 82: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP centeralign> | ||
3. Set the channel A AWG Min value to 0.5 and Max value to 4.5V, Freq = 350 to apply a 4Vp-p square wave centered on 2.5 V as the input voltage to the circuit. From the AWG A Mode drop down menu select the SVMI mode. From the AWG A Shape drop down menus select Square. From the AWG B Mode drop down menu select the Hi-Z mode. | 3. Set the channel A AWG Min value to 0.5 and Max value to 4.5V, Freq = 350 to apply a 4Vp-p square wave centered on 2.5 V as the input voltage to the circuit. From the AWG A Mode drop down menu select the SVMI mode. From the AWG A Shape drop down menus select Square. From the AWG B Mode drop down menu select the Hi-Z mode. | ||
Line 91: | Line 95: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
This configuration allows the oscilloscope to look at the input voltage of the circuit and the current through the inductor on channel A and the output voltage of the circuit on channel B. Make sure you have checked the Sync AWG selector. | This configuration allows the oscilloscope to look at the input voltage of the circuit and the current through the inductor on channel A and the output voltage of the circuit on channel B. Make sure you have checked the Sync AWG selector. | ||
Line 105: | Line 109: | ||
• A Capacitor stores charge. What do you think an Inductor stores? | • A Capacitor stores charge. What do you think an Inductor stores? | ||
Answer in brief. | Answer in brief. | ||
+ | |||
+ | **Resources: | ||
+ | |||
+ | * Fritzing files: [[downgit> | ||
+ | * LTSpice files: [[downgit> | ||
**For Further Reading:** | **For Further Reading:** | ||
- | [[university: | + | [[university: |
+ | [[university: | ||
- | **Return to Lab Activity [[university: | + | **Return to [[university: |
+ | **Return to [[university: | ||