This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:courses:alm1k:circuits1:alm-cir-5 [27 Feb 2018 17:04] – add breadboard figure Doug Mercer | university:courses:alm1k:circuits1:alm-cir-5 [03 Nov 2021 20:14] (current) – [Activity: Transient Response of RC Circuit] Doug Mercer | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity | + | ======Activity: |
=====Objective: | =====Objective: | ||
Line 14: | Line 14: | ||
In this lab activity you will apply a pulse waveform to the RC circuit to analyses the transient response of the circuit. The pulse-width relative to a circuit' | In this lab activity you will apply a pulse waveform to the RC circuit to analyses the transient response of the circuit. The pulse-width relative to a circuit' | ||
- | Time Constant (t): A measure of time required for certain changes in voltages and currents in RC and RL circuits. Generally, when the elapsed time exceeds five time constants (5t) after switching has occurred, the currents and voltages have reached their final value, which is also called steady-state response. | + | Time Constant (τ): Denoted by the Greek letter tau, τ, it represents a measure of time required for certain changes in voltages and currents in RC and RL circuits. Generally, when the elapsed time exceeds five time constants (5τ) after switching has occurred, the currents and voltages have reached their final value, which is also called steady-state response. |
The time constant of an RC circuit is the product of equivalent capacitance and the Thévenin resistance as viewed from the terminals of the equivalent capacitor. | The time constant of an RC circuit is the product of equivalent capacitance and the Thévenin resistance as viewed from the terminals of the equivalent capacitor. | ||
Line 34: | Line 34: | ||
From Kirchhoff' | From Kirchhoff' | ||
- | < | + | < |
- | where, V is the applied source voltage to the circuit | + | where, V is the applied source voltage to the circuit |
{{ : | {{ : | ||
Line 44: | Line 44: | ||
The discharge voltage for the capacitor is given by: | The discharge voltage for the capacitor is given by: | ||
- | < | + | < |
- | Where Vo is the initial voltage stored in capacitor at t = 0, and RC = t is time constant. The response curve is a decaying exponential as shown in figure 3. | + | Where Vo is the initial voltage stored in capacitor at t = 0. |
+ | The product | ||
+ | The response curve is a decaying exponential as shown in figure 3. | ||
{{ : | {{ : | ||
Line 67: | Line 69: | ||
{{ : | {{ : | ||
+ | <WRAP centeralign> | ||
2. Set the channel A AWG Min value to 0.5 and Max value to 4.5V to apply a 4Vp-p square wave centered on 2.5 V as the input voltage to the circuit. From the AWG A Mode drop down menu select the SVMI mode. From the AWG A Shape drop down menus select Square. From the AWG B Mode drop down menu select the Hi-Z mode. | 2. Set the channel A AWG Min value to 0.5 and Max value to 4.5V to apply a 4Vp-p square wave centered on 2.5 V as the input voltage to the circuit. From the AWG A Mode drop down menu select the SVMI mode. From the AWG A Shape drop down menus select Square. From the AWG B Mode drop down menu select the Hi-Z mode. | ||
Line 74: | Line 77: | ||
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
This configuration uses the oscilloscope to look at the input of the circuit on channel A and the output of the circuit on channel B. Make sure you have checked the Sync AWG selector. | This configuration uses the oscilloscope to look at the input of the circuit on channel A and the output of the circuit on channel B. Make sure you have checked the Sync AWG selector. | ||
Line 82: | Line 85: | ||
a. Pulse width >> 5t : Set the frequency of AWG A output such that the capacitor has enough time to fully charge and discharge during each cycle of the square wave. So let the pulse width be 15t and set the frequency according to equation (2). The value you have found should be approximately 15 Hz. Determine the time constant from the waveforms obtained on the screen if you can. If you cannot obtain the time constant easily, explain possible reasons. | a. Pulse width >> 5t : Set the frequency of AWG A output such that the capacitor has enough time to fully charge and discharge during each cycle of the square wave. So let the pulse width be 15t and set the frequency according to equation (2). The value you have found should be approximately 15 Hz. Determine the time constant from the waveforms obtained on the screen if you can. If you cannot obtain the time constant easily, explain possible reasons. | ||
- | b. Pulse width = 5t : Set the frequency such that the pulse width = 5t (this should be approximately 45 Hz). Since the pulse width is 5t, the capacitor should just be able to fully charge and discharge during each pulse cycle. From the figure determine t (see figure 2 and figure | + | b. Pulse width = 5t : Set the frequency such that the pulse width = 5t (this should be approximately 45 Hz). Since the pulse width is 5t, the capacitor should just be able to fully charge and discharge during each pulse cycle. From the figure determine t (see figure 2 and figure |
{{ : | {{ : | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
c. Pulse width << 5t : In this case the capacitor does not have time to charge significantly before it is switched to discharge, and vice versa. Let the pulse width be only 1.0t in this case and set the frequency accordingly. | c. Pulse width << 5t : In this case the capacitor does not have time to charge significantly before it is switched to discharge, and vice versa. Let the pulse width be only 1.0t in this case and set the frequency accordingly. | ||
Line 98: | Line 101: | ||
2. Discuss the effects of changing component values. | 2. Discuss the effects of changing component values. | ||
- | **For Further Reading:** | + | **Resources:** |
- | [[university: | + | * Fritzing files: |
+ | * LTSpice files: [[downgit> | ||
+ | |||
+ | **For Further Reading:** | ||
- | **Return to Lab Activity | + | [[university: |
+ | [[university: | ||
+ | **Return to [[university: | ||
+ | **Return to [[university: |