Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:courses:alm1k:circuits1:alm-cir-15a [03 Nov 2021 20:34] – [Activity 15: DC-DC Boost Converter] Doug Merceruniversity:courses:alm1k:circuits1:alm-cir-15a [05 Nov 2021 14:58] (current) – [Background Basics:] Doug Mercer
Line 1: Line 1:
-======Activity: DC-DC Boost Converter, For ADALM1000======+======Activity: DC-DC Boost Converter ADALM1000======
  
 =====Objective:===== =====Objective:=====
Line 16: Line 16:
  
 When the current flowing in an inductor is quickly interrupted a large voltage spike is observed across the inductor. This large voltage spike can in fact be useful in some cases. One example is the DC to DC boost converter, which is a circuit that can create a larger DC voltage from a smaller one with very high efficiency. The basic idea is to combine an inductive spike generator with a rectifier circuit, as shown in figure 2. Whenever the transistor is abruptly turned off the voltage at the drain spikes up, the diode D<sub>1</sub> is forward biased and current will flow from the inductor to charge up the storage capacitors C<sub>3</sub> and C<sub>4</sub>. When the drain voltage subsequently drops below the voltage on the capacitor, the diode is reverse biased and the output voltage remains constant. Just as in the chapter on AC power supplies, the output capacitor must be sized appropriately to minimize the ripple relating to the current flowing in the load. We will just use a small capacitor here and hence the circuit will not be able to source a large output current.  When the current flowing in an inductor is quickly interrupted a large voltage spike is observed across the inductor. This large voltage spike can in fact be useful in some cases. One example is the DC to DC boost converter, which is a circuit that can create a larger DC voltage from a smaller one with very high efficiency. The basic idea is to combine an inductive spike generator with a rectifier circuit, as shown in figure 2. Whenever the transistor is abruptly turned off the voltage at the drain spikes up, the diode D<sub>1</sub> is forward biased and current will flow from the inductor to charge up the storage capacitors C<sub>3</sub> and C<sub>4</sub>. When the drain voltage subsequently drops below the voltage on the capacitor, the diode is reverse biased and the output voltage remains constant. Just as in the chapter on AC power supplies, the output capacitor must be sized appropriately to minimize the ripple relating to the current flowing in the load. We will just use a small capacitor here and hence the circuit will not be able to source a large output current. 
 +
 +This exercise will expand on these concepts, deriving a converter that “boosts” a low voltage to a high voltage.  Subsequent activities will close the loop around these circuits and examine loop stability and time-domain response.
 +
 +{{page>:university:labs:open_loop_boost_and_buck_adalm2000#Activity 1: An Ideal* Open-Loop Boost Converter Simulation&footer}}
  
 ====Materials:==== ====Materials:====
university/courses/alm1k/circuits1/alm-cir-15a.txt · Last modified: 05 Nov 2021 14:58 by Doug Mercer