This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
university:courses:alm1k:alm-labs-list [22 Sep 2018 03:03] – [Active Learning Module Lab Activities, Electronics I and II] Doug Mercer | university:courses:alm1k:alm-labs-list [04 Oct 2018 16:22] – add link to ADALP2000 wiki page Antoniu Miclaus | ||
---|---|---|---|
Line 7: | Line 7: | ||
In general these example labs are based on the [[university: | In general these example labs are based on the [[university: | ||
- | They are generally written to be performed using just the components provided in the Analog Parts Kit, ADALP2000, supplied through ADI distribution channels, however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page. | + | They are generally written to be performed using just the components provided in the Analog Parts Kit, [[university: |
===Pre-Lab Circuit Simulation=== | ===Pre-Lab Circuit Simulation=== |