Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:courses:alm1k:alm-labs-list [24 Feb 2018 20:28] – Add Comms labs section Doug Mercer | university:courses:alm1k:alm-labs-list [04 Oct 2018 16:22] – add link to ADALP2000 wiki page Antoniu Miclaus |
---|
In general these example labs are based on the [[university:tools:m1k|ADALM1000]] (M1K) entry level design hardware and the accompanying [[university:tools:m1k:alice:desk-top-users-guide|ALICE Desk-Top]] software package. It is also possible to perform these lab activities using the ADALM2000 (M2K) hardware module with minor adjustments to the circuits. [[university:courses:alm1k:m2k-convert-labs|This document]] outlines how the labs might be altered for use with M2K. | In general these example labs are based on the [[university:tools:m1k|ADALM1000]] (M1K) entry level design hardware and the accompanying [[university:tools:m1k:alice:desk-top-users-guide|ALICE Desk-Top]] software package. It is also possible to perform these lab activities using the ADALM2000 (M2K) hardware module with minor adjustments to the circuits. [[university:courses:alm1k:m2k-convert-labs|This document]] outlines how the labs might be altered for use with M2K. |
| |
They are generally written to be performed using just the components provided in the Analog Parts Kit, ADALP2000, supplied through ADI distribution channels, however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page. | They are generally written to be performed using just the components provided in the Analog Parts Kit, [[university:tools:adalp2000:parts-index|ADALP2000]], supplied through ADI distribution channels, however additional devices are sometimes needed. Other sources of components can of course be used and there is additional information on that further down on this page. |
| |
===Pre-Lab Circuit Simulation=== | ===Pre-Lab Circuit Simulation=== |
- [[university:courses:alm1k:alm-lab-gbw|Op-Amp Gain Bandwidth Product]] | - [[university:courses:alm1k:alm-lab-gbw|Op-Amp Gain Bandwidth Product]] |
- [[university:courses:alm1k:alm-lab-comp|The Voltage Comparator]] | - [[university:courses:alm1k:alm-lab-comp|The Voltage Comparator]] |
- [[university:courses:alm1k:alm-lab-2|PN Diode I/V curves]] | - [[university:courses:alm1k:alm-lab-2|PN Diode ]] and [[university:courses:alm1k:alm-lab-zener-diode|Zener Diode]] I/V curves |
- [[university:courses:alm1k:circuits1:alm-cir-diode-rectifier|Diode Rectifiers]] | - [[university:courses:alm1k:circuits1:alm-cir-diode-rectifier|Diode Rectifiers]] |
- [[university:courses:alm1k:circuits1:alm-cir-precision-rectifier|Precision Rectifiers, Absolute value circuits]] | - [[university:courses:alm1k:circuits1:alm-cir-precision-rectifier|Precision Rectifiers, Absolute value circuits]] |
- [[university:courses:alm1k:alm-lab-22|Optocouplers]] ( analog isolation amplifier ) | - [[university:courses:alm1k:alm-lab-22|Optocouplers]] ( analog isolation amplifier ) |
- [[university:courses:alm1k:alm-lab-scr|Silicon Controlled Rectifiers]] | - [[university:courses:alm1k:alm-lab-scr|Silicon Controlled Rectifiers]] |
| - [[university:courses:alm1k:alm-ldo-lab|Low Drop out Linear Voltage Regulators]] |
- [[university:courses:alm1k:alm-lab-15|DC-DC Converters I]] ( inductors ) | - [[university:courses:alm1k:alm-lab-15|DC-DC Converters I]] ( inductors ) |
- [[university:courses:alm1k:alm-lab-16| DC-DC Converters II]] ( capacitors ) | - [[university:courses:alm1k:alm-lab-16| DC-DC Converters II]] ( capacitors ) |