Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
university:courses:alm1k:alm-lab-4 [18 Sep 2019 15:31] – [Questions:] Doug Merceruniversity:courses:alm1k:alm-lab-4 [02 Feb 2023 20:37] (current) – add example I/V curve Doug Mercer
Line 1: Line 1:
-======Activity 4: BJT Characteristic Curves ======+======Activity: BJT Characteristic Curves, For ADALM1000======
  
 =====Objective:===== =====Objective:=====
Line 39: Line 39:
  
 The 0.4 V steps in the voltage driving the 10 KΩ base resistor will produce approximately 0.4 V/10 KΩ or 40 uA steps in the base current. Using the scope in XY mode plot channel CA-V on the horizontal axis (V<sub>CE</sub>) and channel CA-I (I<sub>C</sub>) on the vertical axis. You should see a set of 10 curves of I<sub>C</sub> vs. V<sub>CE</sub>, one for each of the 10 different base current levels. These base current levels should be approximately 0, 40uA, 80uA, 120uA ... 360uA. It may be necessary to slightly adjust the 0.6V offset level of the first step of channel B up or down slightly to insure it is right at the initial turn on value ( I<sub>B</sub>=0 and I<sub>C</sub>=0) of the transistor you are testing. The 0.4 V steps in the voltage driving the 10 KΩ base resistor will produce approximately 0.4 V/10 KΩ or 40 uA steps in the base current. Using the scope in XY mode plot channel CA-V on the horizontal axis (V<sub>CE</sub>) and channel CA-I (I<sub>C</sub>) on the vertical axis. You should see a set of 10 curves of I<sub>C</sub> vs. V<sub>CE</sub>, one for each of the 10 different base current levels. These base current levels should be approximately 0, 40uA, 80uA, 120uA ... 360uA. It may be necessary to slightly adjust the 0.6V offset level of the first step of channel B up or down slightly to insure it is right at the initial turn on value ( I<sub>B</sub>=0 and I<sub>C</sub>=0) of the transistor you are testing.
 +
 +{{ :university:courses:alm1k:alm_lab4_f5.png?400 |}}
 +
 +<WRAP centeralign>Figure 1A, Example NPN I<sub>C</sub> vs. V<sub>CE</sub> characteristic curves.</WRAP>
  
 ====Questions:==== ====Questions:====
Line 55: Line 59:
 {{ :university:courses:alm1k:alm_lab4_f2.png?600 |}} {{ :university:courses:alm1k:alm_lab4_f2.png?600 |}}
  
-<WRAP centeralign>Figure 2 PNP I<sub>C</sub> vs. V<sub>CE</sub> characteristic curve measurments</WRAP>+<WRAP centeralign>Figure 2 PNP I<sub>C</sub> vs. V<sub>CE</sub> characteristic curve measurements</WRAP>
  
 ====NPN Beta vs Collector Voltage Directions:==== ====NPN Beta vs Collector Voltage Directions:====
Line 93: Line 97:
  
 **Resources:** **Resources:**
-  * LTSpice files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m1k/ltspice/bjt_char_curves_ltspice | bjt_char_curves_ltspice]] +  * LTSpice files: [[downgit>education_tools/tree/master/m1k/ltspice/bjt_char_curves_ltspice | bjt_char_curves_ltspice]] 
-  * Fritzing files: [[ https://minhaskamal.github.io/DownGit/#/home?url=https://github.com/analogdevicesinc/education_tools/tree/master/m1k/fritzing/bjt_char_curves_bb | bjt_char_curves_bb]]+  * Fritzing files: [[downgit>education_tools/tree/master/m1k/fritzing/bjt_char_curves_bb | bjt_char_curves_bb]]
  
 **For Further Reading:** **For Further Reading:**
university/courses/alm1k/alm-lab-4.txt · Last modified: 02 Feb 2023 20:37 by Doug Mercer