This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:courses:alm1k:alm-lab-16 [27 Jul 2018 15:26] – [Directions:] Doug Mercer | university:courses:alm1k:alm-lab-16 [03 Jan 2021 22:12] – fix links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ======Activity | + | ======Activity: |
=====Objective: | =====Objective: | ||
Line 11: | Line 11: | ||
Scope traces are similarly referred to by channel and voltage / current. Such as CA-V , CB-V for the voltage waveforms and CA-I , CB-I for the current waveforms. | Scope traces are similarly referred to by channel and voltage / current. Such as CA-V , CB-V for the voltage waveforms and CA-I , CB-I for the current waveforms. | ||
- | The circuits used in this Lab activity while generally low current can produce voltages beyond the 0 to 5 V analog input range of the ALM1000. Input voltage divider techniques as discussed in the document on ALM1000 analog inputs will be required. Refer to the document and construct and use input dividers before preforming any of these experiments with the ALM1000. | + | The circuits used in this Lab activity while generally low current can produce voltages beyond the 0 to 5 V analog input range of the ALM1000. |
=====Concept: | =====Concept: | ||
Line 129: | Line 129: | ||
**For further reading:** | **For further reading:** | ||
+ | [[adi> | ||
http:// | http:// | ||
http:// | http:// | ||
- | http:// | + | [[adi>static/ |
====Appendix: | ====Appendix: |