This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
software:linux:docs:iio:iio [30 May 2012 13:36] – [IIO Ring Buffer] Michael Hennerich | software:linux:docs:iio:iio [23 Feb 2017 13:26] – Fix typo Lars-Peter Clausen | ||
---|---|---|---|
Line 4: | Line 4: | ||
===== IIO Overview ===== | ===== IIO Overview ===== | ||
- | * The Industrial I/O subsystem is intended to provide support for devices that in some sense are analog to digital or digital to analog | + | * The Industrial I/O subsystem is intended to provide support for devices that in some sense are analog to digital or digital to analog |
* Devices that fall into this category are: | * Devices that fall into this category are: | ||
* ADCs | * ADCs | ||
Line 44: | Line 44: | ||
* These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. | * These are similar to input in that they provide a route to user space for hardware triggered events. Such events include threshold detectors, free-fall detectors and more complex action detection. | ||
- | <note> | + | <WRAP round help> |
A given device may have one or more event channel. | A given device may have one or more event channel. | ||
- | </note> | + | </WRAP> |
* Hardware ring buffer support | * Hardware ring buffer support |