Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
software:linux:docs:iio:iio [23 Feb 2017 13:26] – Fix typo Lars-Peter Clausensoftware:linux:docs:iio:iio [05 Jun 2020 17:03] (current) – [IIO Overview] Grammar changes Iulia Moldovan
Line 22: Line 22:
   * The overall aim is to fill the gap between the somewhat similar hwmon and input subsystems.   * The overall aim is to fill the gap between the somewhat similar hwmon and input subsystems.
   * Hwmon is very much directed at low sample rate sensors used in applications such as fan speed control and temperature measurement.   * Hwmon is very much directed at low sample rate sensors used in applications such as fan speed control and temperature measurement.
-  * Input isas it'name suggests focused on human interaction input devices.:+  * The input is⁠ (as its name suggestsfocused on human interaction input devices:
     * Keyboard     * Keyboard
     * Mouse     * Mouse
Line 28: Line 28:
     * Joystick     * Joystick
  
-  * In some cases there is considerable overlap between these and IIO.+  * In some casesthere is considerable overlap between these and IIO.
  
   * A typical device falling into the IIO category would be connected via SPI or I2C.   * A typical device falling into the IIO category would be connected via SPI or I2C.
software/linux/docs/iio/iio.1487852781.txt.gz · Last modified: 23 Feb 2017 13:26 by Lars-Peter Clausen