This is an old revision of the document!
This driver allows any Blackfin system timer to be used as IIO trigger. It supports trigger rates from 0 to 100kHz in Hz resolution.
Configure kernel with “make menuconfig” (alternatively use “make xconfig” or “make qconfig”)
Linux Kernel Configuration Device Drivers ---> [*] Staging drivers ---> <*> Industrial I/O support ---> --- Industrial I/O support -*- Enable ring buffer support within IIO -*- Industrial I/O lock free software ring -*- Enable triggered sampling support [--snip--] *** Triggers - standalone *** < > Periodic RTC triggers < > GPIO trigger < > SYSFS trigger <*> Blackfin TIMER trigger
One or multiple instances of this driver can be declared by adding appropriate platform device data. An example is shown below:
static struct resource iio_bfin_trigger_resources[] = { { .start = IRQ_TIMER3, .end = IRQ_TIMER3, .flags = IORESOURCE_IRQ, }, }; static struct platform_device iio_bfin_trigger = { .name = "iio_bfin_tmr_trigger", .id = 0, .num_resources = ARRAY_SIZE(iio_bfin_trigger_resources), .resource = iio_bfin_trigger_resources, };
static struct platform_device *board_devices[] __initdata = { &iio_bfin_trigger };
static int __init board_init(void) { [--snip--] platform_add_devices(board_devices, ARRAY_SIZE(board_devices)); [--snip--] return 0; } arch_initcall(board_init);
<box 100% green|This specifies any shell prompt running on the target>
root:/> cd sys/bus/iio/devices/ root:/sys/bus/iio/devices> ls device0 device0:buffer0:event0 device1:buffer0:access0 device0:buffer0 device1 device1:buffer0:event0 device0:buffer0:access0 device1:buffer0 trigger0</box>
<box 100% green|This specifies any shell prompt running on the target>
root:/sys/bus/iio/devices> cd trigger0 root:/sys/devices/trigger0> ls name subsystem frequency uevent</box>
<box 100% green|This specifies any shell prompt running on the target>
root:/sys/devices/trigger0> cat name bfintmr3</box>
<box 100% green|This specifies any shell prompt running on the target>
root:/sys/devices/trigger0> echo 1000 > frequency root:/sys/devices/trigger0> echo 0 > frequency</box>