This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
software:linux:docs:iio:iio-trig-bfin-timer [02 Jan 2013 22:19] – eliminate box Robin Getz | software:linux:docs:iio:iio-trig-bfin-timer [05 Feb 2021 15:48] (current) – [More Information] Michael Hennerich | ||
---|---|---|---|
Line 6: | Line 6: | ||
It supports trigger rates from 0 to 100kHz in Hz resolution. | It supports trigger rates from 0 to 100kHz in Hz resolution. | ||
- | <note tip> | + | <WRAP tip> |
This driver depends on BLACKFIN | This driver depends on BLACKFIN | ||
- | </note> | + | </WRAP> |
====== Adding Linux driver support ====== | ====== Adding Linux driver support ====== | ||
Line 108: | Line 108: | ||
- | ====== More Information ====== | ||
- | |