This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:tools:software:ace:understandingtheui:startview [03 Dec 2020 15:44] – John McKane | resources:tools:software:ace:understandingtheui:startview [10 Feb 2021 15:25] (current) – John McKane | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | === Navigation === | ||
+ | You can return to the ACE Application User Guide Homepage here: | ||
+ | **[[resources: | ||
+ | |||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | |||
===== Start View ===== | ===== Start View ===== | ||
- | When the application opens you will be presented with the Start View, Figure 5. This view allows you to set up a | + | When the application opens you will be presented with the Start View. This view allows you to set up a |
system to be used in a session. A system can be made up of a single | system to be used in a session. A system can be made up of a single | ||
or multiple subsystems and can be a mixture of attached hardware and | or multiple subsystems and can be a mixture of attached hardware and | ||
Line 7: | Line 14: | ||
| | ||
{{: | {{: | ||
- | Figure 5: Start View | + | |
==== Attached Hardware Section ==== | ==== Attached Hardware Section ==== | ||
Line 29: | Line 36: | ||
Previous sessions can be opened and new sessions created from the left-hand pane of the Start View, Recently opened sessions can be | Previous sessions can be opened and new sessions created from the left-hand pane of the Start View, Recently opened sessions can be | ||
viewed and opened from the recent sessions’ section. Only one session can be open at a time. | viewed and opened from the recent sessions’ section. Only one session can be open at a time. | ||
+ | |||
{{: | {{: | ||
==== Navigation from the Start View ==== | ==== Navigation from the Start View ==== |