This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:tools:software:ace:understandingtheui:startview [03 Dec 2020 15:43] – created John McKane | resources:tools:software:ace:understandingtheui:startview [10 Feb 2021 15:25] (current) – John McKane | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | === Navigation === | ||
+ | You can return to the ACE Application User Guide Homepage here: | ||
+ | **[[resources: | ||
+ | |||
+ | * [[resources: | ||
+ | * [[resources: | ||
+ | |||
===== Start View ===== | ===== Start View ===== | ||
- | When the application opens you will be presented with the Start View, Figure 5. This view allows you to set up a | + | When the application opens you will be presented with the Start View. This view allows you to set up a |
system to be used in a session. A system can be made up of a single | system to be used in a session. A system can be made up of a single | ||
or multiple subsystems and can be a mixture of attached hardware and | or multiple subsystems and can be a mixture of attached hardware and | ||
Line 6: | Line 13: | ||
| | ||
- | {{: | + | {{: |
==== Attached Hardware Section ==== | ==== Attached Hardware Section ==== | ||
- | The attached hardware section displays all subsystems which are physically | + | The attached hardware section displays all subsystems which are physically |
+ | ched | ||
to the PC through the USB and for which there are plug-ins. The identify | to the PC through the USB and for which there are plug-ins. The identify | ||
hardware button can be used to identify the detected hardware, generally by | hardware button can be used to identify the detected hardware, generally by | ||
Line 29: | Line 36: | ||
Previous sessions can be opened and new sessions created from the left-hand pane of the Start View, Recently opened sessions can be | Previous sessions can be opened and new sessions created from the left-hand pane of the Start View, Recently opened sessions can be | ||
viewed and opened from the recent sessions’ section. Only one session can be open at a time. | viewed and opened from the recent sessions’ section. Only one session can be open at a time. | ||
- | {{ : | + | |
+ | {{: | ||
==== Navigation from the Start View ==== | ==== Navigation from the Start View ==== | ||
The add subsystems button, see Figure 5, adds all selected subsystems local | The add subsystems button, see Figure 5, adds all selected subsystems local |