Differences
This shows you the differences between two versions of the page.
| |
resources:tools-software:uc-drivers:renesas:rx63n_software_design [17 Sep 2012 18:24] – Created. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:rx63n_software_design [18 Sep 2012 09:14] (current) – Added: Disable the main() function generation. Dragos Bogdan |
---|
* In the "//Select Target CPU//" window, select “//RX600//” CPU series, “//RX63N//” CPU Type and press //Next//. | * In the "//Select Target CPU//" window, select “//RX600//” CPU series, “//RX63N//” CPU Type and press //Next//. |
* In the first “//Option Setting//” window change only the Precision of double from single to "//Double precision//" and press //Next//. | * In the first “//Option Setting//” window change only the Precision of double from single to "//Double precision//" and press //Next//. |
* In the second “//Option Setting//” and “//Setting the Content of Files to be generated//” windows keep default settings and press //Next//. | * In the second “//Option Setting//” window keep default settings and press //Next//. |
| * In the “Setting the Content of Files to be generated” window select ”None” for the ”Generate main() Function” option and press Next. |
* In the “//Setting the Standard Library//” window press “Enable all” and then //Next//. | * In the “//Setting the Standard Library//” window press “Enable all” and then //Next//. |
* In the “//Setting the Stack Area//” window check the "//Use User Stack//" option and press //Next//. | * In the “//Setting the Stack Area//” window check the "//Use User Stack//" option and press //Next//. |