Differences
This shows you the differences between two versions of the page.
| Last revisionBoth sides next revision |
resources:tools-software:uc-drivers:renesas:rl78g14_e2studio_software_tutorial [28 Feb 2013 11:03] – created Dan Nechita | resources:tools-software:uc-drivers:renesas:rl78g14_e2studio_software_tutorial [13 Mar 2013 18:36] – Added the Project Summary window message. Dragos Bogdan |
---|
* Run the //**e2studio**// integrated development environment. | * Run the //**e2studio**// integrated development environment. |
* Choose to create a new project (//**File – New –C Project**//). | * Choose to create a new project (//**File – New –C Project**//). |
* Select //**Sample Project**// in Project type section and the //**KPIT GNURL78-ELF**// toolchain. | * Select //**Executable (Renesas) - Sample Project**// type and the //**KPIT GNURL78-ELF**// toolchain. |
* Name the project(//**ADIEvalBoard**// for example) and click //**Next**//. | * Name the project(//**ADIEvalBoard**// for example) and click //**Next**//. |
| |
{{ :resources:tools-software:uc-drivers:renesas:rl78g14_e2studio_2.jpg? |}} | {{ :resources:tools-software:uc-drivers:renesas:rl78g14_e2studio_2.jpg? |}} |
| |
| * Click OK to generate the project when the Project Summary window appears. |
* Open the project’s options window (//**Project – Properties**//). | * Open the project’s options window (//**Project – Properties**//). |
* Select //**Settings**// from the //**C/C++ Build**// category. In the //**Tool Settings**// tab, locate //**Debug level**// field and select //**Level3: Maximum. Allows Macro Debugging(-g3)**// and set the //**Debug format**// field to //**DWARF with GNU extensions**//. Click //**OK**//. | * Select //**Settings**// from the //**C/C++ Build**// category. In the //**Tool Settings**// tab, locate //**Debug level**// field and select //**Level3: Maximum. Allows Macro Debugging(-g3)**// and set the //**Debug format**// field to //**DWARF with GNU extensions**//. Click //**OK**//. |