This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adxl362 [12 Nov 2012 13:59] – Added the round download indicator. Dan Nechita | resources:tools-software:uc-drivers:renesas:adxl362 [22 Jul 2019 09:52] – Update no-OS driver link Andrei Drimbarean | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **ADXL362 Driver: | ||
+ | * **PmodACL2 Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 19: | Line 22: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
* [[http:// | * [[http:// | ||
- | * PmodACL2 | + | * [[http:// |
==== Required Software ==== | ==== Required Software ==== | ||
Line 36: | Line 39: | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the ADXL362 demonstration project on a Renesas RL78G14 platform using the PmodACL2. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The ADXL362 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADXL362 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXL362 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | ==== Hardware Setup ==== | ||
+ | A PmodACL2 has to be connected to the PMOD1 connector (see image below). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | * displays the acceleration values on x, y and z axis; | ||
+ | * displays temperature; | ||
+ | * detects any activity or inactivity supported by the device. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
+ | |||
====== Renesas RX63N Quick Start Guide ====== | ====== Renesas RX63N Quick Start Guide ====== |