Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:adxl345 [12 Nov 2012 10:37] – Removed applilet3 content / updated drivers. Dan Nechitaresources:tools-software:uc-drivers:renesas:adxl345 [24 Jan 2021 17:22] (current) – Fix bad links Dragos Bogdan
Line 3: Line 3:
  
 **HW Platform(s):** **HW Platform(s):**
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] 
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
  
 ===== Downloads ===== ===== Downloads =====
  
-<WRAP round download 30%> +<WRAP round download 80%>
-  * {{:resources:tools-software:uc-drivers:adxl345_generic.zip|ADXL345 Generic Driver}}+
   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}}
   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}}
 +  * **ADXL345 Driver:           ** https://github.com/analogdevicesinc/no-OS/tree/master/drivers/accel/adxl345
 +  * **PmodACL Demo for RL78G14: ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/PmodACL
 +  * **RL78G14 Common Drivers:   ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/Common
 </WRAP> </WRAP>
  
Line 18: Line 20:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]]
   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13)   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13)
  
Line 42: Line 44:
 ==== Software Project Setup ==== ==== Software Project Setup ====
 {{page>rl78g13_software_tutorial_without_applilet3}} {{page>rl78g13_software_tutorial_without_applilet3}}
 +
 +====== Renesas RL78G14 Quick Start Guide ======
 +This section contains a description of the steps required to run the ADXL345 demonstration project on a Renesas RL78G14 platform using the PmodACL.
 +
 +==== Required Hardware ====
 +
 +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g14-yrdkrl78g14-demonstration-kit-rl78g14|Renesas Demo Kit for RL78G14 (Renesas)]]
 +  * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G14)
 +==== Required Software ====
 +  * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
 +  * The ADXL345 demonstration project for the Renesas RL78G14 platform.
 +
 +<WRAP round info 80%>
 +The ADXL345 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXL345 Driver**,  the **PmodACL Demo for RL78G14** and the **RL78G14 Common Drivers**.
 +
 +All three parts have to be downloaded.
 +</WRAP>
 +==== Hardware Setup ====
 +There are two options:
 +
 +  * The ADXL345 part installed on the Renesas Demonstration Kit (RDK) for RL78G14 can be used. In this case, the I2C protocol has to be chosen with 'ADXL345_Init()' function.
 +
 +{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14.jpg? |}}
 +
 +  * A PmodACL can be connected to the PMOD1 connector. In this case, the SPI protocol has to be chosen with 'ADXL345_Init()' function.
 +
 +{{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g14.jpg? |}}
 +
 +==== Reference Project Overview ====
 +The reference project:
 +  * reads and displays the data for each axis on LCD;
 +  * it displays also on LCD if the interrupts “Single Tap”, “Double Tap” or “Free-Fall” were activated. 
 +
 +{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14_screen.jpg? |}}
 +
 +
 +==== Software Project Tutorial ====
 +{{page>rl78g14_software_tutorial}}
 +
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
Line 47: Line 88:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N)   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N)
  
 ==== Required Software ==== ==== Required Software ====
-  * [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]] +  * [[https://www.renesas.com/us/en/software-tool/high-performance-embedded-workshop|High-performance Embedded Workshop for RX62N family]] 
-  * [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]]+  * [[https://www.renesas.com/us/en/software-tool/renesas-peripheral-driver-library|Renesas Peripheral Driver Library for RX62N family]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
resources/tools-software/uc-drivers/renesas/adxl345.1352713024.txt.gz · Last modified: 12 Nov 2012 10:37 by Dan Nechita