Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:adxl345 [28 Sep 2012 13:55] – Removed the Microchip sections. Dragos Bogdanresources:tools-software:uc-drivers:renesas:adxl345 [24 Jan 2021 17:22] (current) – Fix bad links Dragos Bogdan
Line 1: Line 1:
 +====== ADXL345 - No-OS Driver for Renesas Microcontroller Platforms ======
 {{page>:resources:tools-software:uc-drivers:adxl345}} {{page>:resources:tools-software:uc-drivers:adxl345}}
  
 **HW Platform(s):** **HW Platform(s):**
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] 
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
  
 ===== Downloads ===== ===== Downloads =====
-  * {{:resources:tools-software:uc-drivers:adxl345_generic.zip|ADXL345 Generic Driver}}+ 
 +<WRAP round download 80%>
   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}}
   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}}
 +  * **ADXL345 Driver:           ** https://github.com/analogdevicesinc/no-OS/tree/master/drivers/accel/adxl345
 +  * **PmodACL Demo for RL78G14: ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/PmodACL
 +  * **RL78G14 Common Drivers:   ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/Common
 +</WRAP>
  
 ====== Renesas RL78G13 Quick Start Guide ====== ====== Renesas RL78G13 Quick Start Guide ======
Line 14: Line 20:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]]
   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13)   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13)
  
 ==== Required Software ==== ==== Required Software ====
   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
-  * [[http://am.renesas.com/|Applilet3 for RL78G13]] 
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 32: Line 37:
 {{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g13.jpg? |}} {{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g13.jpg? |}}
  
-==== Software Setup ==== +==== Reference Project Overview ==== 
-With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured:+In this example, the output data of each axis is read and displayed on the Renesas Demonstration Kit for RL78G13 board’s LCD. Were also activated “Single Tap”, “Double Tap” and “Free-Fall” interrupts. When one of them occurs, on the LCD screen appears a corresponding message.
  
-=== CSI10 (Clocked Serial Interface 10) – For the ST7579 LCD and the ADXL345 part(if the SPI protocol is chosen) === +{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g13_screen.jpg? |}}
-Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings: +
-  * Transfer mode setting//**Single transfer mode**// +
-  * Data length setting //**8 bits**// +
-  * Transfer direction setting//**MSB**// +
-  * Specification of data timing//**Type 1**// +
-  * Transfer rate setting – Clock mode: //**Internal clock (master)**// +
-  * Transfer rate setting – Baudrate: //**1000000**// (bps) +
-  * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// +
-  * Uncheck the callback functions.+
  
-=== IICA0 (Inter Integrated Circuit Bus) - For the ADXL345 part(if the I2C protocol is chosen) === +==== Software Project Setup ==== 
-Choose the //**Single master**// transfer mode and configure the interface with the following settings: +{{page>rl78g13_software_tutorial_without_applilet3}}
-  * Clock mode setting: //**fCLK/2**// +
-  * Local address setting – Address: //**16**// +
-  * Operation mode setting : //**Standard**// +
-  * Operation mode setting – Transfer clock (fSCL): //**100000**// (bps) +
-  * Interrupt setting – Communication end interrupt priority (INTIICA0): //**Low**// +
-  * Callback function setting: Check //**Master transmission end**// and //**Master reception end**// callback functions +
-  * Callback function enhanced feature setting: Check the //**Callback function enhanced feature setting**//.+
  
-=== TM00 (Timer 00) – For the DelayMs() function ===  +====== Renesas RL78G14 Quick Start Guide ====== 
-Configure TM00 as an interval timer: +This section contains a description of the steps required to run the ADXL345 demonstration project on a Renesas RL78G14 platform using the PmodACL.
-  * Interval timer setting - Interval value(16 bits): //**1**// ms +
-  * Interval timer setting - Uncheck //Generates INTM00 when counting is started// +
-  * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)//+
  
-=== Watchdog Timer === +==== Required Hardware ==== 
-Disable the watchdog timer+ 
-  * Choose for the Watchdog timer operation setting: //**Unused**// option.+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g14-yrdkrl78g14-demonstration-kit-rl78g14|Renesas Demo Kit for RL78G14 (Renesas)]] 
 +  * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G14) 
 +==== Required Software ==== 
 +  * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]] 
 +  The ADXL345 demonstration project for the Renesas RL78G14 platform. 
 + 
 +<WRAP round info 80%> 
 +The ADXL345 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXL345 Driver**,  the **PmodACL Demo for RL78G14** and the **RL78G14 Common Drivers**. 
 + 
 +All three parts have to be downloaded. 
 +</WRAP> 
 +==== Hardware Setup ==== 
 +There are two options: 
 + 
 +  * The ADXL345 part installed on the Renesas Demonstration Kit (RDK) for RL78G14 can be used. In this case, the I2C protocol has to be chosen with 'ADXL345_Init()' function. 
 + 
 +{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14.jpg? |}} 
 + 
 +  * A PmodACL can be connected to the PMOD1 connector. In this case, the SPI protocol has to be chosen with 'ADXL345_Init()' function. 
 + 
 +{{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g14.jpg? |}}
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
-In this example, the output data of each axis is read and displayed on the Renesas Demonstration Kit for RL78G13 board’s LCD. Were also activated “Single Tap”, “Double Tap” and “Free-Fall” interrupts. When one of them occurs, on the LCD screen appears a corresponding message.+The reference project: 
 +  * reads and displays the data for each axis on LCD
 +  * it displays also on LCD if the interrupts “Single Tap”, “Double Tap” or “Free-Fall” were activated
  
-{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g13_screen.jpg? |}}+{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14_screen.jpg? |}} 
 + 
 + 
 +==== Software Project Tutorial ==== 
 +{{page>rl78g14_software_tutorial}}
  
-==== Software Project Setup ==== 
-{{page>rl78g13_software_tutorial}} 
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
Line 78: Line 88:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N)   * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N)
  
 ==== Required Software ==== ==== Required Software ====
-  * [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]] +  * [[https://www.renesas.com/us/en/software-tool/high-performance-embedded-workshop|High-performance Embedded Workshop for RX62N family]] 
-  * [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]]+  * [[https://www.renesas.com/us/en/software-tool/renesas-peripheral-driver-library|Renesas Peripheral Driver Library for RX62N family]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 111: Line 121:
 {{page>rx62n_software_design}} {{page>rx62n_software_design}}
  
 +====== More information ======
 +{{page>:resources:tools-software:uc-drivers:more-information}}
resources/tools-software/uc-drivers/renesas/adxl345.txt · Last modified: 24 Jan 2021 17:22 by Dragos Bogdan