Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:tools-software:uc-drivers:renesas:adxl345 [28 Sep 2012 13:55] – Removed the Microchip sections. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adxl345 [24 Jan 2021 17:05] – Fix bad links Dragos Bogdan |
---|
| ====== ADXL345 - No-OS Driver for Renesas Microcontroller Platforms ====== |
{{page>:resources:tools-software:uc-drivers:adxl345}} | {{page>:resources:tools-software:uc-drivers:adxl345}} |
| |
**HW Platform(s):** | **HW Platform(s):** |
* [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] |
* [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]] |
| |
===== Downloads ===== | ===== Downloads ===== |
* {{:resources:tools-software:uc-drivers:adxl345_generic.zip|ADXL345 Generic Driver}} | |
| <WRAP round download 80%> |
* {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}} | * {{:resources:tools-software:uc-drivers:renesas:adxl345_rl78g13.zip|ADXL345 RL78G13 Driver}} |
* {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}} | * {{:resources:tools-software:uc-drivers:renesas:adxl345_rx62n.zip|ADXL345 RX62N Driver}} |
| * **ADXL345 Driver: ** https://github.com/analogdevicesinc/no-OS/tree/master/drivers/accel/adxl345 |
| * **PmodACL Demo for RL78G14: ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/PmodACL |
| * **RL78G14 Common Drivers: ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/Common |
| </WRAP> |
| |
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== |
| |
==== Required Hardware ==== | ==== Required Hardware ==== |
* [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13) | * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G13) |
| |
==== Required Software ==== | ==== Required Software ==== |
* [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]] | * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]] |
* [[http://am.renesas.com/|Applilet3 for RL78G13]] | |
| |
==== Hardware Setup ==== | ==== Hardware Setup ==== |
{{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g13.jpg? |}} | {{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g13.jpg? |}} |
| |
==== Software Setup ==== | ==== Reference Project Overview ==== |
With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured: | In this example, the output data of each axis is read and displayed on the Renesas Demonstration Kit for RL78G13 board’s LCD. Were also activated “Single Tap”, “Double Tap” and “Free-Fall” interrupts. When one of them occurs, on the LCD screen appears a corresponding message. |
| |
=== CSI10 (Clocked Serial Interface 10) – For the ST7579 LCD and the ADXL345 part(if the SPI protocol is chosen) === | {{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g13_screen.jpg? |}} |
Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings: | |
* Transfer mode setting: //**Single transfer mode**// | |
* Data length setting : //**8 bits**// | |
* Transfer direction setting: //**MSB**// | |
* Specification of data timing: //**Type 1**// | |
* Transfer rate setting – Clock mode: //**Internal clock (master)**// | |
* Transfer rate setting – Baudrate: //**1000000**// (bps) | |
* Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// | |
* Uncheck the callback functions. | |
| |
=== IICA0 (Inter Integrated Circuit Bus) - For the ADXL345 part(if the I2C protocol is chosen) === | ==== Software Project Setup ==== |
Choose the //**Single master**// transfer mode and configure the interface with the following settings: | {{page>rl78g13_software_tutorial_without_applilet3}} |
* Clock mode setting: //**fCLK/2**// | |
* Local address setting – Address: //**16**// | |
* Operation mode setting : //**Standard**// | |
* Operation mode setting – Transfer clock (fSCL): //**100000**// (bps) | |
* Interrupt setting – Communication end interrupt priority (INTIICA0): //**Low**// | |
* Callback function setting: Check //**Master transmission end**// and //**Master reception end**// callback functions | |
* Callback function enhanced feature setting: Check the //**Callback function enhanced feature setting**//. | |
| |
=== TM00 (Timer 00) – For the DelayMs() function === | ====== Renesas RL78G14 Quick Start Guide ====== |
Configure TM00 as an interval timer: | This section contains a description of the steps required to run the ADXL345 demonstration project on a Renesas RL78G14 platform using the PmodACL. |
* Interval timer setting - Interval value(16 bits): //**1**// ms | |
* Interval timer setting - Uncheck //Generates INTM00 when counting is started// | |
* Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | |
| |
=== Watchdog Timer === | ==== Required Hardware ==== |
Disable the watchdog timer: | |
* Choose for the Watchdog timer operation setting: //**Unused**// option. | * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g14/index.jsp|Renesas Demo Kit for RL78G14 (Renesas)]] |
| * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RL78G14) |
| ==== Required Software ==== |
| * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]] |
| * The ADXL345 demonstration project for the Renesas RL78G14 platform. |
| |
| <WRAP round info 80%> |
| The ADXL345 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADXL345 Driver**, the **PmodACL Demo for RL78G14** and the **RL78G14 Common Drivers**. |
| |
| All three parts have to be downloaded. |
| </WRAP> |
| ==== Hardware Setup ==== |
| There are two options: |
| |
| * The ADXL345 part installed on the Renesas Demonstration Kit (RDK) for RL78G14 can be used. In this case, the I2C protocol has to be chosen with 'ADXL345_Init()' function. |
| |
| {{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14.jpg? |}} |
| |
| * A PmodACL can be connected to the PMOD1 connector. In this case, the SPI protocol has to be chosen with 'ADXL345_Init()' function. |
| |
| {{ :resources:tools-software:uc-drivers:renesas:pmod_acl_rl78g14.jpg? |}} |
| |
==== Reference Project Overview ==== | ==== Reference Project Overview ==== |
In this example, the output data of each axis is read and displayed on the Renesas Demonstration Kit for RL78G13 board’s LCD. Were also activated “Single Tap”, “Double Tap” and “Free-Fall” interrupts. When one of them occurs, on the LCD screen appears a corresponding message. | The reference project: |
| * reads and displays the data for each axis on LCD; |
| * it displays also on LCD if the interrupts “Single Tap”, “Double Tap” or “Free-Fall” were activated. |
| |
{{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g13_screen.jpg? |}} | {{ :resources:tools-software:uc-drivers:renesas:adxl345_rl78g14_screen.jpg? |}} |
| |
| |
| ==== Software Project Tutorial ==== |
| {{page>rl78g14_software_tutorial}} |
| |
==== Software Project Setup ==== | |
{{page>rl78g13_software_tutorial}} | |
| |
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |
| |
==== Required Hardware ==== | ==== Required Hardware ==== |
* [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] | * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]] |
* [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N) | * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=PMOD-ACL|PmodACL]] (optional, because an ADXL345 part is installed on Renesas Demonstration Kit (RDK) for RX62N) |
| |
==== Required Software ==== | ==== Required Software ==== |
* [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]] | * [[https://www.renesas.com/us/en/software-tool/high-performance-embedded-workshop|High-performance Embedded Workshop for RX62N family]] |
* [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]] | * [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]] |
| |
{{page>rx62n_software_design}} | {{page>rx62n_software_design}} |
| |
| ====== More information ====== |
| {{page>:resources:tools-software:uc-drivers:more-information}} |