This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adxl345 [01 Jun 2012 12:51] – Added the "More Information" section Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adxl345 [19 Jul 2012 09:38] – ADXL345 added for MC7 Dragos Bogdan | ||
---|---|---|---|
Line 18: | Line 18: | ||
* [[http:// | * [[http:// | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
===== Driver Description ===== | ===== Driver Description ===== | ||
Line 180: | Line 182: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Digilent Cerebot MC7 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the ADXL345 demonstration project on a Digilent Cerebot MC7 platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodACL can be connected to the J6 connector of Cerebot MC7 development board for I2C operation, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | or to the JB connector of Cerebot MC7 development board for SPI operation. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | Following commands were implemented in this version of AD7991 reference project for Cerebot MC7 board. | ||
+ | ^ Command ^ Description ^ | ||
+ | | help? | Displays all available commands. | | ||
+ | | communication= | Selects the communication interface. Accepted values: 0(I2C), | ||
+ | | communication? | ||
+ | | acceleration? | ||
+ | | interrupts? | Displays the state of the interrupts. | | ||
+ | |||
+ | Commands can be executed using a serial terminal connected to the UART1 peripheral of dsPIC33FJ128MC706A. | ||
+ | |||
+ | The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. | ||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page>: | ||
====== More information ====== | ====== More information ====== | ||
{{page> | {{page> |