Wiki

No renderer 'pdf' found for mode 'pdf'
This version (24 Jan 2021 17:55) was approved by Dragos Bogdan.The Previously approved version (24 Jan 2021 17:44) is available.Diff

ADT7420 - No-OS Driver for Renesas Microcontroller Platforms

Supported Devices

Evaluation Boards

Overview

The ADT7420 is a high accuracy digital temperature sensor offering breakthrough performance over a wide industrial range, housed in an LFCSP package. It contains a band gap temperature reference and a 13-bit ADC to monitor and digitize the temperature to a 0.0625°C resolution. The ADC resolution, by default, is set to 13 bits (0.0625°C). This can be changed to 16 bits (0.0078°C) by setting Bit 7 in the configuration register to 1 (Register Address 0x03). The ADT7420 is guaranteed to operate over supply voltages from 2.7 V to 5.5 V. Operating at 3.3 V, the average supply current is typically 210 μA. The ADT7420 has a shutdown mode that powers down the device and offers a shutdown current of typically 2 μA. The ADT7420 is rated for operation over the −40°C to +150°C temperature range.

Pin A0 and Pin A1 are available for address selection, giving the ADT7420 four possible I2C addresses. The CT pin is an open-drain output that becomes active when the temperature exceeds a programmable critical temperature limit. The default critical temperature limit is 147°C. The INT pin is also an open-drain output that becomes active when the temperature exceeds a programmable limit. The INT and CT pins can operate in either comparator or interrupt mode.

Applications

  • RTD and thermistor replacement
  • Medical equipment
  • Cold junction compensation
  • Industrial control and test
  • Food transportation and storage
  • Environmental monitoring and HVAC

28 Sep 2012 16:29 · Dragos Bogdan

The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for different microcontroller platforms.

Driver Description

The driver contains two parts:

  • The driver for the ADT7420 part, which may be used, without modifications, with any microcontroller.
  • The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements the communication with the device and hides the actual details of the communication protocol to the ADI driver.

The Communication Driver has a standard interface, so the ADT7420 driver can be used exactly as it is provided.

There are three functions which are called by the ADT7420 driver:

  • I2C_Init() – initializes the communication peripheral.
  • I2C_Write() – writes data to the device.
  • I2C_Read() – reads data from the device.

I2C driver architecture

The implementation of these three functions depends on the used microcontroller.

The following functions are implemented in this version of ADT7420 driver:

Function Description
unsigned char ADT7420_GetRegisterValue(unsigned char registerAddress) Reads the value of a register.
void ADT7420_SetRegisterValue(unsigned char registerAddress, unsigned char registerValue) Sets the value of a register.
char ADT7420_Init(void) Initializes the comm. peripheral and checks if the device is present.
void ADT7420_Reset(void) Resets the ADT7420.
void ADT7420_SetOperationMode(unsigned char mode) Sets the operational mode for ADT7420.
void ADT7420_SetResolution(unsigned char resolution) Sets the resolution for ADT7420.
float ADT7420_GetTemperature(void) Reads the temperature data and converts it to Celsius degrees.
01 Oct 2012 15:27 · Dragos Bogdan

Downloads

Renesas RL78G13 Quick Start Guide

This section contains a description of the steps required to run the ADT7420 demonstration project on a Renesas RL78G13 platform using the PmodTMP2.

Required Hardware

Required Software

Hardware Setup

A PmodTMP2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G13:

  PmodTMP2 J1 connector Pin SCL → YRDKRL78G13 J9 connector Pin 1
  PmodTMP2 J1 connector Pin SDA → YRDKRL78G13 J9 connector Pin 3
  PmodTMP2 J1 connector Pin GND → YRDKRL78G13 J11 connector Pin 5
  PmodTMP2 J1 connector Pin VCC → YRDKRL78G13 J11 connector Pin 6

Reference Project Overview

The reference project:

  • reads the temperature from the device;
  • displays the temperature on the LCD in degrees Celsius.

Software Project Tutorial

This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G13 for controlling and monitoring the operation of the ADI part.

  • Run the IAR Embedded Workbench for Renesas RL78 integrated development environment.
  • Choose to create a new project (Project – Create New Project).
  • Select the RL78 tool chain, the Empty project template and click OK.

  • Select a location and a name for the project (ADIEvalBoard for example) and click Save.

  • Open the project’s options window (Project – Options).
  • From the Target tab of the General Options category select the RL78 – R5F100LE device.

  • From the Setup tab of the Debugger category select the TK driver and click OK.

  • Extract the files from the lab .zip archive and copy them into the project’s folder.

  • The new source files have to be included into the project. Open the Add Files… window (Project – Add Files…), select all the copied files and click open.

  • At this moment, all the files are included into the project.
  • The project is ready to be compiled and downloaded on the board. Press the F7 key to compile it. Press CTRL + D to download and debug the project.
  • A window will appear asking to configure the emulator. Keep the default settings and press OK.

  • To run the project press F5.

03 Sep 2012 13:02 · Dragos Bogdan

Renesas RL78G14 Quick Start Guide

This section contains a description of the steps required to run the ADT7420 demonstration project on a Renesas RL78G14 platform using the PmodTMP2.

Required Hardware

Required Software

The ADT7420 demonstration project for the Renesas RL78G14 platform consists of three parts: the ADT7420 Driver, the PmodTMP2 Demo for RL78G14 and the RL78G14 Common Drivers.

All three parts have to be downloaded.

Hardware Setup

A PmodTMP2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14:

  PmodTMP2 J1 connector Pin SCL → RDKRL78G14 J8 connector Pin 1
  PmodTMP2 J1 connector Pin SDA → RDKRL78G14 J8 connector Pin 3
  PmodTMP2 J1 connector Pin GND → RDKRL78G14 J11 connector Pin 5
  PmodTMP2 J1 connector Pin VCC → RDKRL78G14 J11 connector Pin 6

Reference Project Overview

The reference project:

  • reads the temperature from the device;
  • displays the temperature on the LCD in degrees Celsius.

Software Project Tutorial

This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RL78G14 for controlling and monitoring the operation of the ADI part.

  • Run the IAR Embedded Workbench for Renesas RL78 integrated development environment.
  • Choose to create a new project (Project – Create New Project).
  • Select the RL78 tool chain, the Empty project template and click OK.

  • Select a location and a name for the project (ADIEvalBoard for example) and click Save.

  • Open the project’s options window (Project – Options).
  • From the Target tab of the General Options category select the RL78 – R5F104PJ device.

  • From the Setup tab of the Debugger category select the TK driver and click OK.

  • Copy the downloaded files into the project's folder.

  • The new source files have to be included into the project. Open the Add Files… window (Project – Add Files…), select all the copied files and click open.

  • At this moment, all the files are included into the project.
  • The project is ready to be compiled and downloaded on the board. Press the F7 key to compile it. Press CTRL + D to download and debug the project.
  • A window will appear asking to configure the emulator. Keep the default settings and press OK.

  • To run the project press F5.

09 May 2013 17:10 · Dragos Bogdan

Renesas RX63N Quick Start Guide

This section contains a description of the steps required to run the ADT7420 demonstration project on a Renesas RX63N platform using the PmodTMP2.

Required Hardware

Required Software

Hardware Setup

A PmodCDC1 has to be interfaced with the Renesas Demonstration Kit (RDK) for RX63N:

PmodCDC1 J1 connector Pin SCL ? YRDKRX63N J2 connector Pin 1
PmodCDC1 J1 connector Pin SDA ? YRDKRX63N J2 connector Pin 3
PmodCDC1 J1 connector Pin GND ? YRDKRX63N J15 connector Pin 5
PmodCDC1 J1 connector Pin VCC ? YRDKRX63N J15 connector Pin 6

Reference Project Overview

The reference project reads the temperature from the device and displays it on the LCD.

Software Project Setup

This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RX63N for controlling and monitoring the operation of the ADI part.

  • Run the High-performance Embedded Workshop integrated development environment.
  • A window will appear asking to create or open project workspace. Choose “Create a new project workspace” option and press OK.
  • From “Project Types” option select “Application”, name the Workspace and the Project “ADIEvalBoard”, select the “RX” CPU family and “Renesas RX Standard” tool chain. Press OK.

  • A few windows will appear asking to configure the project:
    • In the “Select Target CPU” window, select “RX600” CPU series, “RX63N” CPU Type and press Next.
    • In the first “Option Setting” window change only the Precision of double from single to “Double precision” and press Next.
    • In the second “Option Setting” window keep default settings and press Next.
    • In the “Setting the Content of Files to be generated” window select ”None” for the ”Generate main() Function” option and press Next.
    • In the “Setting the Standard Library” window press “Enable all” and then Next.
    • In the “Setting the Stack Area” window check the “Use User Stack” option and press Next.
    • In the “Setting the Vector” window keep default settings and press Next.
    • In the “Setting the Target System for Debugging” window choose “RX600 Segger J-Link” target and press Next.
    • In the “Setting the Debugger Options” and “Changing the Files Name to be created” windows keep default settings, press Next and Finish.
  • The workspace is created.

  • The RPDL (Renesas Peripheral Driver Library) has to integrated in the project. Unzip the RPDL files (double-click on the file “RPDL_RX63N.exe”). Navigate to where the RPDL files were unpacked and double-click on the “Copy_RPDL_RX63N.bat” to start the copy process. Choose the 100 pins package and little endian option, type the full path where the project was created and after the files were copied, press any key to close the window.
  • The new source files have to be included in the project. Use the key sequence Alt, P, A to open the “Add files to project ‘ADIEvalBoard’” window. Double click on the RPDL folder. From the “Files of type” drop-down list, select “C source file (*.C)”. Select all of the files and press Add.

  • To avoid conflicts with standard project files remove the files “intprg.c” and “vecttbl.c” which are included in the project. Use the key sequence Alt, P, R to open the “Remove Project Files” window. Select the files, click on Remove and press OK.

  • Next the new directory has to be included in the project. Use the key sequence Alt, B, R to open the “RX Standard Toolchain” window. Select the C/C++ tab, select “Show entries for: Include file directories” and press Add. Select “Relative to: Project directory”, type “RPDL” as sub-directory and press OK.

  • The library file path has to be added in the project. Select the Link/Library tab, select “Show entries for: Library files” and press Add. Select “Relative to: Project directory”, type “RPDL\RX63N_library” as file path and press OK.

  • Because the “intprg.c” file was removed the “PIntPrg” specified in option “start” has to be removed. Change “Category” to “Section”. Press “Edit”, select “PIntPRG” and press “Remove”. From this window the address of each section can be also modified. Set the second address to 0xFFF00000 and the third one to 0xFFF00100. After all the changes are made press OK two times.

  • At this point the files extracted from the zip file located in the “Software Tools” section have to be added into the project. Copy all the files from the archive into the project folder.

  • Now, the files have to be included in the project. Use the key sequence Alt, P, A to open the “Add files to project ‘ADIEvalBoard’” window. Navigate into ADI folder. From the “Files of type” drop-down list, select “Project Files”. Select all the copied files and press Add.

  • Now, the project is ready to be built. Press F7. The message after the Build Process is finished has to be “0 Errors, 0 Warnings”. To run the program on the board, you have to download the firmware into the microprocessor’s memory.
17 Sep 2012 18:24 · Dragos Bogdan

More information

01 Jun 2012 12:17
resources/tools-software/uc-drivers/renesas/adt7420.txt · Last modified: 24 Jan 2021 17:55 by Dragos Bogdan