This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adp5589 [12 Nov 2012 15:08] – Removed applilet3 content / updated drivers. Dan Nechita | resources:tools-software:uc-drivers:renesas:adp5589 [29 May 2013 14:30] – added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads Lucian Sin | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **ADP5589 Driver: | ||
+ | * **PmodIOXP Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 36: | Line 39: | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project waits for a password to unlock the keypad. | + | The reference project: |
+ | * waits for a password to unlock the keypad; | ||
+ | |||
{{ : | {{ : | ||
- | After the keypad is unlocked the state of the pin R0 and the key presses are displayed on the LCD. Also the PWM generator is enabled on pin R3. | + | * after the keypad is unlocked, it will display on the LCD the last pressed key and the status of R0 pin; also the PWM generator is enabled on pin R3. |
{{ : | {{ : | ||
Line 46: | Line 50: | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the ADP5589 demonstration project on a Renesas RL78G14 platform using the PmodIOXP. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The ADP5589 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADP5589 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADP5589 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodIOXP has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14: | ||
+ | |||
+ | PmodIOXP J3 connector 1 (SCL) → RDKRL78G14 J8 connector Pin 1 | ||
+ | PmodIOXP J3 connector 3 (SDA) → RDKRL78G14 J8 connector Pin 3 | ||
+ | PmodIOXP J3 connector 5 (GND) → RDKRL78G14 J11 connector Pin 5 | ||
+ | PmodIOXP J3 connector 7 (VCC) → RDKRL78G14 J11 connector Pin 6 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project: | ||
+ | * waits for a password to unlock the keypad; | ||
+ | | ||
+ | {{ : | ||
+ | |||
+ | * after the keypad is unlocked, it will display on the LCD the last pressed and released key(which can be different keys) and the status of R0 pin; also the PWM generator is enabled on pin R3. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |