This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adp5589 [01 Oct 2012 16:56] – Removed the Microchip sections. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adp5589 [29 May 2013 14:30] – added RENESAS RL78G14 QUICK START GUIDE and RL78G14 source code downloads Lucian Sin | ||
---|---|---|---|
Line 7: | Line 7: | ||
===== Downloads ===== | ===== Downloads ===== | ||
+ | |||
+ | <WRAP round download 80%> | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **ADP5589 Driver: | ||
+ | * **PmodIOXP Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
+ | </ | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 21: | Line 27: | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
- | * [[http:// | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 33: | Line 38: | ||
{{ : | {{ : | ||
- | ==== Software Setup ==== | + | ==== Reference Project Overview |
- | With the //**Applilet3 | + | The reference project: |
+ | | ||
+ | |||
+ | {{ : | ||
- | === CSI10 (Clocked Serial Interface 10) – For the ST7579 | + | * after the keypad is unlocked, it will display on the LCD the last pressed key and the status |
- | Choose to generate | + | |
- | * Transfer mode setting: //**Single transfer mode**// | + | |
- | * Data length setting : //**8 bits**// | + | |
- | * Transfer direction setting: // | + | |
- | * Specification | + | |
- | * Transfer rate setting – Clock mode: // | + | |
- | * Transfer rate setting – Baudrate: // | + | |
- | * Interrupt setting – Transfer interrupt priority (INTCSI10): // | + | |
- | * Uncheck | + | |
- | === IICA0 (Inter Integrated Circuit Bus) - For the ADP5589 part === | + | {{ :resources:tools-software:uc-drivers:renesas:adp5589_rl78g13_screen_2.jpg? |}} |
- | Choose the //**Single master**// transfer mode and configure the interface with the following settings: | + | |
- | * Clock mode setting: // | + | |
- | * Local address setting – Address: // | + | |
- | * Operation mode setting : // | + | |
- | * Operation mode setting – Transfer clock (fSCL): // | + | |
- | * Interrupt setting – Communication end interrupt priority (INTIICA0): // | + | |
- | * Callback function setting: Check //**Master transmission end**// and //**Master reception end**// callback functions | + | |
- | * Callback function enhanced feature setting: Check the // | + | |
- | === TM00 (Timer 00) – For the DelayMs() function | + | ==== Software Project Tutorial ==== |
- | Configure TM00 as an interval timer: | + | {{page> |
- | * Interval timer setting - Interval value(16 bits): //**1**// ms | + | |
- | * Interval timer setting - Uncheck //Generates INTM00 when counting is started// | + | |
- | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | + | |
- | === Watchdog Timer === | + | ====== Renesas RL78G14 Quick Start Guide ====== |
- | Disable | + | This section contains a description of the steps required to run the ADP5589 demonstration project on a Renesas RL78G14 platform using the PmodIOXP. |
- | * Choose | + | |
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http://www.digilentinc.com/ | ||
+ | | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | | ||
+ | | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The ADP5589 demonstration project for the Renesas RL78G14 platform consists of three parts: the **ADP5589 Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </WRAP> | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | A PmodIOXP has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14: | ||
+ | |||
+ | PmodIOXP J3 connector 1 (SCL) → RDKRL78G14 J8 connector Pin 1 | ||
+ | PmodIOXP J3 connector 3 (SDA) → RDKRL78G14 J8 connector Pin 3 | ||
+ | PmodIOXP J3 connector 5 (GND) → RDKRL78G14 J11 connector Pin 5 | ||
+ | PmodIOXP J3 connector 7 (VCC) → RDKRL78G14 J11 connector Pin 6 | ||
+ | |||
+ | {{ : | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
- | The reference project waits for a password to unlock the keypad. | + | The reference project: |
+ | * waits for a password to unlock the keypad; | ||
+ | |||
+ | {{ : | ||
- | {{ : | + | * after the keypad is unlocked, it will display on the LCD the last pressed and released key(which can be different keys) and the status of R0 pin; also the PWM generator is enabled on pin R3. |
- | After the keypad is unlocked the state of the pin R0 and the key presses are displayed on the LCD. Also the PWM generator is enabled on pin R3. | + | {{ : |
- | {{ : | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
- | {{page>rl78g13_software_tutorial}} | + | {{page>rl78g14_software_tutorial}} |
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |