This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adn2850 [06 Apr 2012 13:17] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adn2850 [25 Jan 2021 05:24] – update renesas links after their web site update Robin Getz | ||
---|---|---|---|
Line 16: | Line 16: | ||
**HW Platform(s): | **HW Platform(s): | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
+ | * [[https:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
The driver contains two parts: | The driver contains two parts: | ||
Line 47: | Line 47: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
Line 52: | Line 53: | ||
==== Required Hardware ==== | ==== Required Hardware ==== | ||
- | * [[http://am.renesas.com/ | + | * [[https://www.renesas.com/ |
* [[adi> | * [[adi> | ||
Line 66: | Line 67: | ||
EVAL-ADN2850SDZ A connector Pin SDO_BF | EVAL-ADN2850SDZ A connector Pin SDO_BF | ||
EVAL-ADN2850SDZ A connector Pin SCLK_BF | EVAL-ADN2850SDZ A connector Pin SCLK_BF | ||
- | EVAL-ADN2850SDZ A connector Pin RDY (RDY) → YRDKRL78G13 J11 connector Pin 7 | ||
EVAL-ADN2850SDZ A connector Pin RESET_BF (Reset) | EVAL-ADN2850SDZ A connector Pin RESET_BF (Reset) | ||
EVAL-ADN2850SDZ A connector Pin WP_BF (WP) → YRDKRL78G13 J11 connector Pin 10 | EVAL-ADN2850SDZ A connector Pin WP_BF (WP) → YRDKRL78G13 J11 connector Pin 10 | ||
Line 105: | Line 105: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | |||
+ | This section contains a description of the steps required to run the ADN2850 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[https:// | ||
+ | * [[adi> | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[https:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | An EVAL-ADN2850SDZ has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: | ||
+ | |||
+ | EVAL-ADN2850SDZ A connector Pin SYNC_BF | ||
+ | EVAL-ADN2850SDZ A connector Pin DIN_BF | ||
+ | EVAL-ADN2850SDZ A connector Pin SDO_BF | ||
+ | EVAL-ADN2850SDZ A connector Pin SCLK_BF | ||
+ | EVAL-ADN2850SDZ A connector Pin RESET_BF (Reset) | ||
+ | EVAL-ADN2850SDZ A connector Pin WP_BF (WP) → YRDKRX62N JN1 connector Pin 17 | ||
+ | EVAL-ADN2850SDZ A connector Pin MUX-A0 | ||
+ | EVAL-ADN2850SDZ A connector Pin MUX-A1 | ||
+ | EVAL-ADN2850SDZ A connector Pin MUX-A2 | ||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project initializes the device, reads the tolerance from EEMEM, and then sets RDAC1 output resistance to the value displayed on the lcd. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | |||
+ | ====== More information ====== | ||
+ | {{page> |