This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:adis16227 [28 Feb 2012 21:57] – Approved Dragos Bogdan | resources:tools-software:uc-drivers:renesas:adis16227 [16 Nov 2012 16:46] – [Evaluation Boards] fixup eval board link Lars-Peter Clausen | ||
---|---|---|---|
Line 5: | Line 5: | ||
===== Evaluation Boards ===== | ===== Evaluation Boards ===== | ||
- | * [[adi> | + | * [[adi>EVAL-ADIS16227|ADIS16227/ |
===== Overview ===== | ===== Overview ===== | ||
Line 16: | Line 16: | ||
**HW Platform(s): | **HW Platform(s): | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
===== Driver Description ===== | ===== Driver Description ===== | ||
The driver contains two parts: | The driver contains two parts: | ||
Line 50: | Line 50: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * {{: | ||
====== Renesas RL78G13 Quick Start Guide ====== | ====== Renesas RL78G13 Quick Start Guide ====== | ||
- | This section contains a description of the steps required to run the ADF4118 | + | This section contains a description of the steps required to run the ADIS16227 |
==== Required Hardware ==== | ==== Required Hardware ==== | ||
Line 60: | Line 61: | ||
==== Required Software ==== | ==== Required Software ==== | ||
* [[http:// | * [[http:// | ||
+ | * [[http:// | ||
==== Hardware Setup ==== | ==== Hardware Setup ==== | ||
Line 73: | Line 75: | ||
{{ : | {{ : | ||
+ | |||
+ | ==== Software Setup ==== | ||
+ | With the // | ||
+ | |||
+ | === CSI10 (Clocked Serial Interface 10) – For the ADIS16227 part and the ST7579 LCD === | ||
+ | Choose to generate the Transmit/ | ||
+ | * Transfer mode setting: //**Single transfer mode**// | ||
+ | * Data length setting : //**8 bits**// | ||
+ | * Transfer direction setting: //**MSB**// | ||
+ | * Specification of data timing: //**Type 1**// | ||
+ | * Transfer rate setting – Clock mode: // | ||
+ | * Transfer rate setting – Baudrate: // | ||
+ | * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// | ||
+ | * Uncheck the callback functions. | ||
+ | |||
+ | === TM00 (Timer 00) – For the DelayMs() function === | ||
+ | Configure TM00 as an interval timer: | ||
+ | * Interval timer setting - Interval value(16 bits): //**1**// ms | ||
+ | * Interval timer setting - Uncheck //Generates INTM00 when counting is started// | ||
+ | * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)// | ||
+ | |||
+ | === Watchdog Timer === | ||
+ | Disable the watchdog timer: | ||
+ | * Choose for the Watchdog timer operation setting: // | ||
==== Reference Project Overview ==== | ==== Reference Project Overview ==== | ||
Line 80: | Line 106: | ||
==== Software Project Setup ==== | ==== Software Project Setup ==== | ||
- | {{page>rl78g13_software_design}} | + | {{page>rl78g13_software_tutorial}} |
+ | |||
+ | ====== Renesas RX62N Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RX62N platform. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[adi> | ||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Hardware Setup ==== | ||
+ | An ADIS16227/ | ||
+ | |||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | ADIS16227/ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | ==== Software Project Setup ==== | ||
+ | {{page> | ||
+ | ====== More information ====== | ||
+ | {{page> |