Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
Next revisionBoth sides next revision
resources:tools-software:uc-drivers:renesas:adis16227 [28 Feb 2012 17:08] – Added the "Downloads" section. Dragos Bogdanresources:tools-software:uc-drivers:renesas:adis16227 [16 Nov 2012 16:46] – [Evaluation Boards] fixup eval board link Lars-Peter Clausen
Line 5: Line 5:
  
 ===== Evaluation Boards ===== ===== Evaluation Boards =====
-  * [[adi>ADIS16227 | ADIS16227/PCBZ]]+  * [[adi>EVAL-ADIS16227|ADIS16227/PCBZ]]
  
 ===== Overview ===== ===== Overview =====
Line 16: Line 16:
 **HW Platform(s):** **HW Platform(s):**
   * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]   * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]]
 +  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]]
 ===== Driver Description ===== ===== Driver Description =====
 The driver contains two parts: The driver contains two parts:
Line 50: Line 50:
   * {{:resources:tools-software:uc-drivers:renesas:adis16227_generic.zip|ADIS16227 Generic Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adis16227_generic.zip|ADIS16227 Generic Driver}}
   * {{:resources:tools-software:uc-drivers:renesas:adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}   * {{:resources:tools-software:uc-drivers:renesas:adis16227_rl78g13.zip|ADIS16227 RL78G13 Driver}}
 +  * {{:resources:tools-software:uc-drivers:renesas:adis16227_rx62n.zip|ADIS16227 RX62N Driver}}
  
 ====== Renesas RL78G13 Quick Start Guide ====== ====== Renesas RL78G13 Quick Start Guide ======
-This section contains a description of the steps required to run the ADF4118 demonstration project on a Renesas RL78G13 platform. +This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RL78G13 platform. 
  
 ==== Required Hardware ==== ==== Required Hardware ====
Line 60: Line 61:
 ==== Required Software ==== ==== Required Software ====
   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
 +  * [[http://am.renesas.com/|Applilet3 for RL78G13]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
Line 73: Line 75:
  
 {{ :resources:tools-software:uc-drivers:renesas:adis16227_pcbz_rl78g13.jpg? |}} {{ :resources:tools-software:uc-drivers:renesas:adis16227_pcbz_rl78g13.jpg? |}}
 +
 +==== Software Setup ====
 +With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured:
 +
 +=== CSI10 (Clocked Serial Interface 10) – For the ADIS16227 part and the ST7579 LCD ===
 +Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings:
 +  * Transfer mode setting: //**Single transfer mode**//
 +  * Data length setting : //**8 bits**//
 +  * Transfer direction setting: //**MSB**//
 +  * Specification of data timing: //**Type 1**//
 +  * Transfer rate setting – Clock mode: //**Internal clock (master)**//
 +  * Transfer rate setting – Baudrate: //**1000000**// (bps)
 +  * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**//
 +  * Uncheck the callback functions.
 +
 +=== TM00 (Timer 00) – For the DelayMs() function === 
 +Configure TM00 as an interval timer:
 +  * Interval timer setting - Interval value(16 bits): //**1**// ms
 +  * Interval timer setting - Uncheck //Generates INTM00 when counting is started//
 +  * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)//
 +
 +=== Watchdog Timer ===
 +Disable the watchdog timer:
 +  * Choose for the Watchdog timer operation setting: //**Unused**// option.
  
 ==== Reference Project Overview ==== ==== Reference Project Overview ====
Line 80: Line 106:
  
 ==== Software Project Setup ==== ==== Software Project Setup ====
-{{page>rl78g13_software_design}}+{{page>rl78g13_software_tutorial}} 
 + 
 +====== Renesas RX62N Quick Start Guide ====== 
 +This section contains a description of the steps required to run the ADIS16227 demonstration project on a Renesas RX62N platform. 
 + 
 +==== Required Hardware ==== 
 +  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] 
 +  * [[adi>ADIS16227 | ADIS16227/PCBZ (Analog Devices)]] 
 +==== Required Software ==== 
 +  * [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]] 
 +  * [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]] 
 + 
 +==== Hardware Setup ==== 
 +An ADIS16227/PCBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N: 
 + 
 +    ADIS16227/PCBZ J1 connector Pin 3 (CS)   → YRDKRX62N J8 connector Pin 15 
 +    ADIS16227/PCBZ J1 connector Pin 6 (MOSI) → YRDKRX62N J8 connector Pin 19 
 +    ADIS16227/PCBZ J1 connector Pin 4 (MISO) → YRDKRX62N J8 connector Pin 22 
 +    ADIS16227/PCBZ J1 connector Pin 2 (SCLK) → YRDKRX62N J8 connector Pin 20 
 +    ADIS16227/PCBZ J1 connector Pin 1 (RST)  → YRDKRX62N JN1 connector Pin 16 
 +    ADIS16227/PCBZ J1 connector Pin 7 (GND)  → YRDKRX62N J8 connector Pin 4 
 +    ADIS16227/PCBZ J1 connector Pin 10 (VCC) → YRDKRX62N J8 connector Pin 3 
 + 
 +{{ :resources:tools-software:uc-drivers:renesas:adis16227_rx62n.jpg? |}} 
 + 
 +==== Reference Project Overview ==== 
 +The reference project runs an offset correction operation, configures the REC_CTRL register and initiates a Manual Time recording. After the process is finished on the LCD are displayed the internal temperature, the power supply voltage and the first value of each axis's buffer. 
 + 
 +{{ :resources:tools-software:uc-drivers:renesas:adis16227_rx62n_screen.jpg? |}} 
 + 
 +==== Software Project Setup ==== 
 +{{page>rx62n_software_design}}
  
 +====== More information ======
 +{{page>more-information}}
resources/tools-software/uc-drivers/renesas/adis16227.txt · Last modified: 25 Jan 2021 05:24 by Robin Getz