This is an old revision of the document!
ADAS1000 - Microcontroller No-OS Driver
Supported Devices
Evaluation Boards
Overview
The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms.
HW Platform(s):
Driver Description
The driver contains two parts:
The driver for the ADAS1000 part, which may be used, without modifications, with any microcontroller.
The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements the communication with the device and hides the actual details of the communication protocol to the
ADI driver.
The Communication Driver has a standard interface, so the ADAS1000 driver can be used exactly as it is provided.
There are three functions which are called by the ADAS1000 driver:
SPI_Init() – initializes the communication peripheral.
SPI_Write() – writes data to the device.
SPI_Read() – reads data from the device.
The following functions are implemented in this version of ADAS1000 driver:
Function | Description |
unsigned char ADAS1000_Init(unsigned long rate) | Initializes the communication with ADAS1000 and checks if the device is present. |
void ADAS1000_GetRegisterValue(unsigned char regAddress, unsigned long* regVal) | Reads the value of a ADAS1000 register. |
void ADAS1000_SetRegisterValue(unsigned char regAddress, unsigned long regVal) | Writes a value into a ADAS1000 register. |
void ADAS1000_SoftwareReset(void) | Performs a software reset of the ADAS1000 |
void ADAS1000_SetInactiveFrameWords(unsigned long wordsMask) | Selects which words are not included in a data frame. |
void ADAS1000_SetFrameRate(unsigned long rate) | Sets the frame rate |
void ADAS1000_ReadData(unsigned char* pDataBuffer, unsigned long frameCnt, unsigned char startRead, unsigned char stopRead, unsigned char waitForReady, unsigned char readyRepeat) | Reads the specified number of frames |
unsigned long ADAS1000_ComputeFrameCrc(unsigned char *pBuf) | Computes the CRC for a frame |
Downloads
Renesas RX62N Quick Start Guide
This section contains a description of the steps required to run the ADAS1000 demonstration project on a Renesas RX62N platform.
Required Hardware
Required Software
Hardware Setup
An EVAL-ADAS1000EBZ board has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
EVAL-ADAS1000EBZ J5 connector Pin DGND → YRDKRX62N J8 connector Pin 4 (GND)
EVAL-ADAS1000EBZ J4 connector Pin 10 (SCLK) → YRDKRX62N LCD1 connector Pin 12 (SCLK)
EVAL-ADAS1000EBZ J4 connector Pin 8 (CSB_0) → YRDKRX62N LCD1 connector Pin 11 (CS)
EVAL-ADAS1000EBZ J4 connector Pin 7 (SDO_0) → YRDKRX62N LCD1 connector Pin 14 (MISO)
EVAL-ADAS1000EBZ J4 connector Pin 4 (SDI_0) → YRDKRX62N LCD1 connector Pin 13 (MOSI)
Reference Project Overview
The following examples are implemented in the reference project:
Example on how to read and write a register;
Example how to start the ADCs Converting and begin streaming ECG data from ADAS1000 at 2kHz rate;
Example on how to Enable Respiration;
Example on how to enable DC Leads Off;
Example on how to enable Shield Amplifier;
Example on how to change the number of words in a frame;
Example on how to configure device and start streaming ECG data at 2kHz rate with Leads off enabled, respiration enabled;
Example on how to configure device and start streaming ECG data at 16kHz rate;
Example on how to configure device and start streaming ECG data at 128kHz rate.
The reference project also configures the 150Hz test tone Sinewave on each ECG channel, stores 1000 frames and sends data through the SCI port. The frames do not contain the Pace, Respiration Magnitude, Respiration Phase, Leads Off Status, GPIO and CRC words.
The format of the data transferred through the SCI port.
Software Project Setup
This section presents the steps for developing a software application that will run on the Renesas Demo Kit for RX62N for controlling and monitoring the operation of the ADI part.
Run the High-performance Embedded Workshop integrated development environment.
A window will appear asking to create or open project workspace. Choose “Create a new project workspace” option and press OK.
From “Project Types” option select “Application”, name the Workspace and the Project “ADIEvalBoard”, select the “RX” CPU family and “Renesas RX Standard” tool chain. Press OK.
The RPDL (Renesas Peripheral Driver Library) has to integrated in the project. Unzip the RPDL files (double-click on the file “RPDL_RX62N.exe”). Navigate to where the RPDL files were unpacked and double-click on the “Copy_RPDL_RX62N.bat” to start the copy process. Choose the LQFP package, type the full path where the project was created and after the files were copied, press any key to close the window.
The new source files have to be included in the project. Use the key sequence Alt, P, A to open the “Add files to project ‘ADIEvalBoard’” window. Double click on the RPDL folder. From the “Files of type” drop-down list, select “C source file (*.C)”. Select all of the files and press Add.
To avoid conflicts with standard project files remove the files “intprg.c” and “vecttbl.c” which are included in the project. Use the key sequence Alt, P, R to open the “Remove Project Files” window. Select the files, click on Remove and press OK.
Next the new directory has to be included in the project. Use the key sequence Alt, B, R to open the “RX Standard Toolchain” window. Select the C/C++ tab, select “Show entries for: Include file directories” and press Add. Select “Relative to: Project directory”, type “RPDL” as sub-directory and press OK.
The library file path has to be added in the project. Select the Link/Library tab, select “Show entries for: Library files” and press Add. Select “Relative to: Project directory”, type “RPDL\RX62N_library” as file path and press OK.
Because the “intprg.c” file was removed the “PIntPrg” specified in option “start” has to be removed. Change “Category” to “Section”. Press “Edit”, select “PIntPRG” and press “Remove”. From this window the address of each section can be also modified. After all the changes are made press OK two times.
Now, the files have to be included in the project. Use the key sequence
Alt, P, A to open the “
Add files to project ‘ADIEvalBoard’” window. Navigate into
ADI folder. From the “
Files of type” drop-down list, select “
Project Files”. Select all the copied files and press
Add.
Now, the project is ready to be built. Press F7. The message after the Build Process is finished has to be “0 Errors, 0 Warnings”. To run the program on the board, you have to download the firmware into the microprocessor’s memory.