This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:tools-software:uc-drivers:renesas:ad7991 [07 Nov 2012 15:31] – Removed applilet3 content / updated drivers. Dragos Bogdan | resources:tools-software:uc-drivers:renesas:ad7991 [29 May 2013 11:29] – [Hardware Setup] Lucian Sin | ||
---|---|---|---|
Line 8: | Line 8: | ||
===== Downloads ===== | ===== Downloads ===== | ||
- | <WRAP round download | + | <WRAP round download |
* {{: | * {{: | ||
* {{: | * {{: | ||
* {{: | * {{: | ||
+ | * **AD799x Driver: | ||
+ | * **PmodAD2 Demo for RL78G14: ** https:// | ||
+ | * **RL78G14 Common Drivers: | ||
</ | </ | ||
Line 42: | Line 45: | ||
==== Software Project Tutorial ==== | ==== Software Project Tutorial ==== | ||
{{page> | {{page> | ||
+ | |||
+ | ====== Renesas RL78G14 Quick Start Guide ====== | ||
+ | This section contains a description of the steps required to run the AD7991 demonstration project on a Renesas RL78G14 platform using the PmodAD2. | ||
+ | |||
+ | ==== Required Hardware ==== | ||
+ | * [[http:// | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Required Software ==== | ||
+ | * [[http:// | ||
+ | * The AD7991 demonstration project for the Renesas RL78G14 platform. | ||
+ | |||
+ | <WRAP round info 80%> | ||
+ | The AD7991 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD799x Driver**, | ||
+ | |||
+ | All three parts have to be downloaded. | ||
+ | </ | ||
+ | ==== Hardware Setup ==== | ||
+ | A PmodAD2 has to be interfaced with the Renesas Demonstration Kit (RDK) for RL78G14: | ||
+ | |||
+ | PmodAD2 J1 connector Pin SCL → RDKRL78G14 J8 connector Pin 1 | ||
+ | PmodAD2 J1 connector Pin SDA → RDKRL78G14 J8 connector Pin 3 | ||
+ | PmodAD2 J1 connector Pin GND → RDKRL78G14 J11 connector Pin 5 | ||
+ | PmodAD2 J1 connector Pin VCC → RDKRL78G14 J11 connector Pin 6 | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | * Using JP1 jumper you can either have 4 input channels or 3 input channels. | ||
+ | \\ | ||
+ | </ | ||
+ | |||
+ | ==== Reference Project Overview ==== | ||
+ | |||
+ | The reference project: | ||
+ | * initiates continuous conversions for all four channels; | ||
+ | * the results of all conversions are displayed on the LCD. | ||
+ | <WRAP round important 80%> | ||
+ | \\ | ||
+ | * The reference voltage for the AD7991 is the supply voltage which is 3.3V. | ||
+ | \\ | ||
+ | </ | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | |||
+ | ==== Software Project Tutorial ==== | ||
+ | {{page> | ||
+ | |||
+ | |||
====== Renesas RX62N Quick Start Guide ====== | ====== Renesas RX62N Quick Start Guide ====== |