Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:tools-software:uc-drivers:renesas:ad7980 [11 Jul 2012 09:09] – Approved Dragos Bogdanresources:tools-software:uc-drivers:renesas:ad7980 [27 Jan 2021 23:00] (current) – use interwiki links Robin Getz
Line 1: Line 1:
-====== AD7980 - Microcontroller No-OS Driver ======+====== AD7980 - No-OS Driver for Renesas Microcontroller Platforms ====== 
 +{{page>:resources:tools-software:uc-drivers:ad7980}}
  
-===== Supported Devices ===== +**HW Platform(s):** 
-  * [[adi>AD7980]]+  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] 
 +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]]
  
-===== Evaluation Boards ===== +===== Downloads =====
-  * PmodAD4+
  
-===== Overview =====+<WRAP round download round 80%> 
 +  * {{:resources:tools-software:uc-drivers:ad7980_generic.zip|AD7980 Generic Driver}} 
 +  * {{:resources:tools-software:uc-drivers:renesas:ad7980_rl78g13.zip|AD7980 RL78G13 Driver}} 
 +  * {{:resources:tools-software:uc-drivers:renesas:ad7980_rx62n.zip|AD7980 RX62N Driver}} 
 +  * **AD7980 Driver:            ** https://github.com/analogdevicesinc/no-OS/tree/master/drivers/adc/ad7980 
 +  * **[[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] Demo for RL78G14: ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/PmodAD4 
 +  * **RL78G14 Common Drivers:   ** https://github.com/analogdevicesinc/no-OS/tree/master/Renesas/RL78G14/Common 
 +</WRAP>
  
-The [[adi>AD7980]] is a 16-bit, successive approximation, analog-to-digital converter (ADC) that operates from a single power supply, VDD. It contains a low power, high speed, 16-bit sampling ADC and a versatile serial interface port. On the CNV rising edge, it samples an analog input IN+ between 0 V to REF with respect to a ground sense IN−. The reference voltage, REF, is applied externally and can be set independent of the supply voltage, VDD. Its power scales linearly with throughput.+====== Renesas RL78G13 Quick Start Guide ====== 
 +This section contains a description of the steps required to run the AD7980 demonstration project on Renesas RL78G13 platform.
  
-{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4.jpg? |}}+==== Required Hardware ==== 
 +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g13-yrdkrl78g13-demonstration-kit-rl78g13|Renesas Demo Kit for RL78G13 (Renesas)]] 
 +  * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]]
  
-The goal of this project (Microcontroller No-OS) is to be able to provide reference projects for lower end processors, which can't run Linux, or aren't running a specific operating system, to help those customers using microcontrollers with ADI parts. Here you can find a generic driver which can be used as a base for any microcontroller platform and also specific drivers for Renesas platforms.+==== Required Software ==== 
 +  * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
  
-**HW Platform(s):** +==== Hardware Setup ==== 
-  [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] +[[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] +
-  * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=CEREBOT-MX3CK|Digilent Cerebot MX3cK (Digilent)]]+
  
-===== Driver Description ===== +{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g13.jpg? |}}
-The driver contains two parts: +
-  * The driver for the AD7980 part, which may be used, without modifications, with any microcontroller. +
-  * The Communication Driver, where the specific communication functions for the desired type of processor and communication protocol have to be implemented. This driver implements the communication with the device and hides the actual details of the communication protocol to the ADI driver.+
  
-The Communication Driver has a standard interface, so the AD7980 driver can be used exactly as it is provided. +<WRAP round important round 80%> 
- +\\ 
-There are three functions which are called by the AD7980 driver: +  * If you want to use AVDD > DVDD (= 3.3Vthen JP3 on PmodAD4 must be removedThe range for AVDD is 3.0V ≤ AVDD ≤ 5.5V
-  * SPI_Init() – initializes the communication peripheral. +\\
-  * SPI_Write(– writes data to the device. +
-  * SPI_Read() – reads data from the device. +
- +
-{{ :resources:tools-software:uc-drivers:renesas:spi_architecture.png? |}} +
-<WRAP centeralign> +
-SPI driver architecture+
 </WRAP> </WRAP>
  
-The following functions are implemented in this version of AD7980 driver: +==== Reference Project Overview ====
-^ Function       ^ Description     ^ +
-| unsigned char AD7980_Init(void) | Initializes the communication peripheral. | +
-| unsigned short AD7980_Conversion(void) | Initiates conversion and reads data. |+
  
-This version of AD7980 driver uses the //**CS Mode 4-Wirewithout Busy Indicator **// mode; the device has to be connected to an SPI-compatible digital host as following:+The reference project: 
 +  * samples the input voltage; 
 +  displays the value on the LCD (in hexadecimal and volts).
  
-  * The AD7980 CNV signal (C2 on the oscilloscope) has to be connected to the SPI MOSI signal+<WRAP round important 80%> 
-  * The AD7980 SDI signal (C1 on the oscilloscope) has to be connected to the SPI CS signal (Chip Select has to be controlled manually). +  * The reference voltage for the AD7980 is 2.5V
-  * The AD7980 SCK signal (C4 on the oscilloscope) has to be connected to the SPI SCK signal. +  * If you want to use another reference voltage, you will need to modify the vRef parameter in ‘AD7980_ConvertToVolts()’ function from ‘PmodAD4.c’. The range for VREF is 2.4V ≤ VREF ≤ 5.1V.
-  * The AD7980 SDO signal (C3 on the oscilloscope) has to be connected to the SPI MISO signal. +
- +
-{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_signals.jpg? |}} +
-<WRAP centeralign> +
-Signals generated by the driver on the SPI port+
 </WRAP> </WRAP>
  
-===== Downloads ===== +{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g13_screen.jpg?200 |}}
-  * {{:resources:tools-software:uc-drivers:renesas:ad7980_generic.zip|AD7980 Generic Driver}} +
-  * {{:resources:tools-software:uc-drivers:renesas:ad7980_rl78g13.zip|AD7980 RL78G13 Driver}} +
-  * {{:resources:tools-software:uc-drivers:renesas:ad7980_rx62n.zip|AD7980 RX62N Driver}} +
-  * {{:resources:tools-software:uc-drivers:microchip:ad7980_pic32.zip|AD7980 PIC32 Driver}}+
  
-====== Renesas RL78G13 Quick Start Guide ====== +==== Software Project Tutorial ==== 
-This section contains a description of the steps required to run the AD7980 demonstration project on a Renesas RL78G13 platform.+{{page>rl78g13_software_tutorial_without_applilet3}} 
 + 
 +====== Renesas RL78G14 Quick Start Guide ====== 
 +This section contains a description of the steps required to run the AD7980 demonstration project on a Renesas RL78G14 platform using the [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]].
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrl78g13/index.jsp|Renesas Demo Kit for RL78G13 (Renesas)]] +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rl78-low-power-8-16-bit-mcus/yrdkrl78g14-yrdkrl78g14-demonstration-kit-rl78g14|Renesas Demo Kit for RL78G14 (Renesas)]] 
-  * PmodAD4+  * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]]
  
 ==== Required Software ==== ==== Required Software ====
   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]   * [[http://www.iar.com/en/Products/IAR-Embedded-Workbench/Renesas-RL78/|IAR Embedded Workbench for Renesas RL78 Kickstart]]
-  * [[http://am.renesas.com/|Applilet3 for RL78G13]]+  * The AD7980 demonstration project for the Renesas RL78G14 platform.
  
 +<WRAP round info 80%>
 +The AD7980 demonstration project for the Renesas RL78G14 platform consists of three parts: the **AD7980 Driver**,  the **[[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] Demo for RL78G14** and the **RL78G14 Common Drivers**.
 +
 +All three parts have to be downloaded.
 +</WRAP>
 ==== Hardware Setup ==== ==== Hardware Setup ====
-PmodAD4 has to be connected to the PMOD1 connector.+[[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be connected to the PMOD1 connector, pins 1 to 6 (see image below).
  
-{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g13.jpg? |}}+{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g14.jpg? |}}
  
-==== Software Setup ==== +<WRAP round important round 80%> 
-With the //**Applilet3 for RL78G13**// tool the following peripherals have to be configured:+\\ 
 +    If you want to use AVDD > DVDD (= 3.3V) then JP3 on PmodAD4 must be removed. The range for AVDD is 3.0V ≤ AVDD ≤ 5.5V. 
 +\\ 
 +</WRAP>
  
-=== CSI10 (Clocked Serial Interface 10) – For the AD7980 part and the ST7579 LCD === +The reference project
-Choose to generate the Transmit/receive function for the CSI10 and configure the interface with the following settings+  * samples the input voltage; 
-  * Transfer mode setting: //**Single transfer mode**// +  * displays the value on the LCD (in hexa, decimal and volts).
-  * Data length setting : //**8 bits**// +
-  * Transfer direction setting: //**MSB**// +
-  * Specification of data timing: //**Type 3**// +
-  * Transfer rate setting – Clock mode: //**Internal clock (master)**// +
-  * Transfer rate setting – Baudrate: //**1000000**// (bps) +
-  * Interrupt setting – Transfer interrupt priority (INTCSI10): //**Low**// +
-  * Uncheck the callback functions.+
  
-=== TM00 (Timer 00) – For the DelayMs() function ===  +<WRAP round important 80%>
-Configure TM00 as an interval timer: +
-  * Interval timer setting - Interval value(16 bits): //**1**// ms +
-  * Interval timer setting - Uncheck //Generates INTM00 when counting is started// +
-  * Interrupt setting - Uncheck // End of timer channel 0 count, generate an interrupt (INTM00)//+
  
-=== Watchdog Timer === +  * The reference voltage for the AD7980 is 2.5V. 
-Disable the watchdog timer: +  * If you want to use another reference voltage, you will need to modify the vRef parameter in ‘AD7980_ConvertToVolts()’ function from ‘PmodAD4.c’. The range for VREF is 2.4V ≤ VREF ≤ 5.1V.
-  * Choose for the Watchdog timer operation setting: //**Unused**// option.+
  
-==== Reference Project Overview ==== +</WRAP> 
-The reference project initiates conversions and reads the captured data from the AD7980.+ 
 +{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g14_screen.jpg? |}}
  
-{{ :resources:tools-software:uc-drivers:renesas:pmod_ad4_rl78g13_screen.jpg? |}} 
  
 ==== Software Project Tutorial ==== ==== Software Project Tutorial ====
-{{page>rl78g13_software_tutorial}}+{{page>rl78g14_software_tutorial}}
  
 ====== Renesas RX62N Quick Start Guide ====== ====== Renesas RX62N Quick Start Guide ======
Line 112: Line 102:
  
 ==== Required Hardware ==== ==== Required Hardware ====
-  * [[http://am.renesas.com/products/tools/introductory_evaluation_tools/renesas_demo_kits/yrdkrx62n/index.jsp|Renesas Demo Kit for RX62N (Renesas)]] +  * [[https://www.renesas.com/us/en/products/microcontrollers-microprocessors/rx-32-bit-performance-efficiency-mcus/yrdkrx62n-yrdkrx62n-demonstration-kit-rx62n|Renesas Demo Kit for RX62N (Renesas)]] 
-  * PmodAD4+  * [[adi>PulsarPMODs|EVAL-AD7980-PMDZ]]
  
 ==== Required Software ==== ==== Required Software ====
-  * [[http://www.renesas.com/products/tools/ide/ide_hew/index.jsp|High-performance Embedded Workshop for RX62N family]] +  * [[https://www.renesas.com/us/en/software-tool/high-performance-embedded-workshop|High-performance Embedded Workshop for RX62N family]] 
-  * [[http://am.renesas.com/products/tools/middleware_and_drivers/c_driver_gen/driver_gen_rpdl/index.jsp|Renesas Peripheral Driver Library for RX62N family]]+  * [[https://www.renesas.com/us/en/software-tool/renesas-peripheral-driver-library|Renesas Peripheral Driver Library for RX62N family]]
  
 ==== Hardware Setup ==== ==== Hardware Setup ====
-PmodAD4 has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:+[[adi>PulsarPMODs|EVAL-AD7980-PMDZ]] has to be interfaced with the Renesas Demonstration Kit (RDK) for RX62N:
  
     PmodAD4 Pin 1 (CS)   → YRDKRX62N J8 connector Pin 15     PmodAD4 Pin 1 (CS)   → YRDKRX62N J8 connector Pin 15
Line 136: Line 126:
 ==== Software Project Setup ==== ==== Software Project Setup ====
 {{page>rx62n_software_design}} {{page>rx62n_software_design}}
- 
-====== Digilent Cerebot MX3cK Quick Start Guide ====== 
-This section contains a description of the steps required to run the AD7980 demonstration project on a Digilent Cerebot MX3cK platform. 
- 
-==== Required Hardware ==== 
-  * [[http://www.digilentinc.com/Products/Detail.cfm?Prod=CEREBOT-MX3CK|Cerebot MX3cK (Digilent)]] 
-  * PmodAD4 
- 
-==== Required Software ==== 
-  * [[http://www.microchip.com/mplabx|MPLAB X Integrated Development Environment]] 
-  * [[http://www.microchip.com/mplabxc|MPLAB XC32 compiler]] 
- 
-==== Hardware Setup ==== 
-A PmodAD4 has to be connected to the JE connector of Cerebot MX3cK development board. 
- 
-{{ :resources:tools-software:uc-drivers:microchip:pmod_ad4_pic32.jpg? |}} 
- 
-==== Reference Project Overview ==== 
-Following commands were implemented in this version of AD7980 reference project for Cerebot MX3cK board. 
-^ Command ^ Description ^ 
-| help? | Displays all available commands. | 
-| voltage? | Initiates a conversion and displays the captured voltage. | 
-| register? | Initiates a conversion and displays the raw data in decimal format. | 
- 
-Commands can be executed using a serial terminal connected to the UART1 peripheral of PIC32MX320F128H. 
- 
-The following image shows a list of commands in a serial terminal connected to processor’s UART peripheral. 
-{{ :resources:tools-software:uc-drivers:microchip:terminal_pic32.png? |}} 
- 
-==== Software Project Setup ==== 
-{{page>:resources:tools-software:uc-drivers:microchip:pic32_software_design}} 
  
 ====== More information ====== ====== More information ======
-{{page>more-information}}+{{page>:resources:tools-software:uc-drivers:more-information}}
resources/tools-software/uc-drivers/renesas/ad7980.txt · Last modified: 27 Jan 2021 23:00 by Robin Getz